Music Shield and Wiznet Ethernet shield

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, salmanfarisvp, violet, jeremy882, crail.lyu969

Post Reply
genhung
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 30, 2012 2:20 pm

Music Shield and Wiznet Ethernet shield

Post by genhung » Fri Mar 30, 2012 2:28 pm

Hi there,

I have just received the following items from Seeed Studio

(1) Music Shield (INT109B2P)
(2) Wiznet Ethernet shield -w5100 (ARD124B2P)

Are these two boards compatible to each other?
How can I joint them together onto an Arduino MEGA board?

Please help.

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Music Shield and Wiznet Ethernet shield

Post by deray » Sat Mar 31, 2012 12:01 pm

Hi~
You can try to weld Female header on the Wiznet Ethernet shield.Hope this help to you.


Best regards,
deray

genhung
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 30, 2012 2:20 pm

Re: Music Shield and Wiznet Ethernet shield

Post by genhung » Sat Mar 31, 2012 1:33 pm

thanks deray
It sounds to me I can put Ethernet shield on the MEGA, then MUSIC shield on the Ether shield. Is it?
Is it fine for not connecting ISP (6pin::MISO\SCK\RST\VCC\HOSI\GND) to Music Shield??
Thanks again!

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Music Shield and Wiznet Ethernet shield

Post by deray » Sat Mar 31, 2012 2:17 pm

Yes,it is.
ISP interface is kept for bringing SPI port when using with Mega , so you should be connected it to MEGA ISP .

best regards,
deray

genhung
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Fri Mar 30, 2012 2:20 pm

Re: Music Shield and Wiznet Ethernet shield

Post by genhung » Wed Apr 04, 2012 9:56 am

hi deray

If both Music Shield and Wiznet Ethernet shield need ISP interface for talking to MEGA,
When I joint these two shield together, will it cause conflicts???

Thanks

User avatar
deray
Elementary-3
Elementary-3
Posts: 327
Joined: Fri Mar 30, 2012 1:45 pm

Re: Music Shield and Wiznet Ethernet shield

Post by deray » Mon Apr 09, 2012 10:24 am

yeah,you can joint these two shield together. but you must change the on of the D10 (Used for SPI Chip Select.pin) , because both of them use the same chip select.ping.

Post Reply