Picture #4 goes with previous post.
Lygra wrote…
“What is interesting is that these steps are in the same time domain as the switching noise of the interlace mode. This may indicate that display issues are causing these steps in the interleave mode, and not the interleave mode itself”
I think these steps are simply the sample steps. I notice you have both chA and chB on so the unit is not interleaving two sets of samples. To see the interleaving effect, you have to “HIDE” chB. Then you will see the sawtooth effect discussed elsewhere and you will notice an apparent doubling of timebase rate. (which I consider advantageous)
Also apparent on jpg 4 is poor risetime and rounding due to the effect of excessive compensation capacitors discussed earlier. After adjusting my values, I acheive a risetime within 2 sample periods for a 3.5MHz waveform of this amplitude. Go on Lygra, get you soldering iron in the back there!
It is quite possible that those are sampling steps as you stated. If you look at the Nano 50Khz square wave display (attached) you will see 25 steps in the display during one sample time = 1us. This square wave on the Nano is a similar percentage of sample rate as the 3.55Mhz on the Quad. Maybe BenF could comment on the reason for these 25 steps in the Nano. I suspect that they are display update steps. Could the Quad processor be running fast enough that you can’t see it’s display update steps?
I know about the interleave display issues and I am trying to keep this thread on bandwidth topic, that is why that info and associated pictures were not included.
I am going to hold off on the soldering iron while I conduct further testing on the factory issued Quad.
bielec
What hardware did you modify (2.2 or 2.6)?
I have just received my V2.60 DSO Quad and want to get the best performance possible. Is it worth me repeating your mods?
Thanks, Dave
Flyingdave,
My quad was the latest version. If you are using the scope for audio measurements then you won’t notice any improvement by modifying it. The changes improve the upper frequency response and risetime on some of the voltage ranges. You would notice this when using the scope near the upper end of the frequency scale. The mods are fiddly so only attempt them if you are confident using a miniature soldering iron.
Bielec
Thanks. I might give it a try - my main use for the Quad is to look at PAL Video, so it would be good if 4.43 MHz wasn’t too far down (<3db).
What size smd components did you use - most of my stock is 0805, which is probably too big?
Dave
I actually used a mixture of 1206 and 0805 s/m capacitors and for the smaller values I used two pieces of thin single core teflon insulated wire tightly twisted together. This arrangement could be adjusted to give best response.
Hi,
Finally, what’s the BW of the quad ?
Thanks
Well, mine stock had 3dB anywhere from 400kHz to 1Mhz depending on the vertical scale selection.
After patching up the front end the 3dB is now shy of 11Mhz for vertical scale settings. I implemented similar to bielec’s solution (almost the same). The parts I used are low drift resistors (25ppm 0603) and NP0 0603 capacitors.
Anyone has example traces for >2Mhz?
When I hook up a signal (which I think is) >1.x MHz, I dont see the trace (flat), but the frequency counter says 2.x Mhz.
Thanks!
geshsoft
What resistors did you change? bielec only mentioned capacitors.
Thanks
Dave
flyingdave my bad about the resistors - I changed 2 and reverted back to the original as they made no difference, so it is just capacitors really.
ATTENTION, DO NOT BOTHER PERFORMING THE MOD BELOW. I just did it and I still have a damn sine wave on my screen when wave out is set to square wave at 6-8MHz (no improvement). How disappointing. This scope is pretty much worthless above 1 MHz. So much for the quad
Noname, a square wave is not a good merit to justify that the mod does nothing.
After the modification the analog BW rolloff is extended to around 10MHz…
In other words, the effective sampling rate of the quad as well as the analog BW of the front end is not good enough to accurately display a square wave at these frequencies. The “sharp edges” of a square wave (higher harmonics) will be attenuated and you will end up mostly with the fundamental.
If you want to be looking at a fully featured square wave you would probably need a scope with way higher analog BW and sampling rate.
Furthermore, although my B channel still worked after the mod, my A channel was nothing but static. I put C73 back on and this got rid of the static but then there was ZERO signal. Nothing but a flat line no matter what. If Seeedstudio has a spare board or suggestions, please let me know.
The mod was not worth doing, and now my A channel is not working. I will probably need to replace an expensive IC and this device was ridiculously expensive as it is. Is there anyone on the planet willing to bothering opening theirs up and risking likelyhood of the plastic case not sealing completely back up again when they could just sell the damn thing and wait for a MUCH better portable scope somewhere down the road?
As far as any signal “improvement” on the remaining B channel, I see basically none. The limitations at 2MHz and above are obvious before and after the mod. Frankly this leads people to believe it is possible to fix the gaping flaws in this device when it is not. I would almost suspect that bielec may have had his silkscreen labeled with components in different positions, but this seems unlikely.
Noname, I agree that the device specs were overstated - both the analog BW and sampling rate.
However, I disagree that the mod posted by bielec is misleading.
bielec stated:
“I now get about 10MHz sinewave bandwidth on all ranges and good pulse response with minimal overshoot and rounding. Trigger and good display of sub 100nS pulses is now possible. As delivered, the scope had less than 1MHz B.W. and poor risetime which varied depending on range.”
Notice that he mentions sine wave BW, which is what should really be used to justify these results. I already explained the reason why you would not see a nice square wave at 6 or 8MHz.
As a matter of fact I performed very similar mod using 0603 parts and got very similar results - my 3dB was shy of 11MHz. However, I would hardly expact this BW to provide a nice sharp looking 8MHz square wave. My TDS210 would do it with no issue, but the analog BW is 60MHz with 1GS/s sampling rate.
Yes, the QUAD has many flaws - you are correct, but as far as being rediculously expansive I don’t think so. A decent Fluke RMS DVM would cost as much or more and has far less capabilities than even immature QUAD.
In any case, this is just my 2c…
The problem with the quad is that when you are only seeing an decent representation of the waveform you are supposed to see at about 1MHz or less, this is a great limitation to the usefulness of the device. The nano seems to have about the same useful bandwidth, I bought the quad hoping it would be a big improvement over the cheaper nano, it was not. Neither of these devices suit my needs. The wave out on the quad goes up to 8MHz in square wave mode, so out of the box, as is, you would expect it to perform like a good scope should up to at least 8MHz. Sadly, this is not the case. I think the reason why there are no more application or firmware updates to this project is that developers already understand their efforts are better used elsewhere. I wish the merchants selling these (including seeedstudio) would advertise upfront in bold type the 1MHz or less bandwidth limitation so people are tempted into thinking as I had that this might actually be a useful tool for their >1MHz applications.
Some reason stop me to go on with this device:
- bandwidth ,not only the poor limitation but also the non-Smoothness gain ,this make calibration can not be achieved.
- FPGA firmware bug, this case triggering not reliable. No development tools I can get to improve it.
- No way to use a debug tool like J-link to debug MCU sourceware. this make Inefficient to develop an application.
Really hope the bug in Quad can much more less than my in English.
It is now getting to the point where I am going to be asking Seeed for my money back.
This device was clearly misrepresented when sold to me and several months down the line my patience is beginning to wear thin. I believe I have given Seeed plenty of time to resolve some of the very basic problems but they have failed so far to do even that. I have also offered to aid them with suggestions and developed a PC client to make the device more useful.
Perhaps it is not Seeed’s fault that this device is clearly never going to do what it was stated it would but they should have been responsible for making sure of that before selling it to me and many other disappointed clients out there.
For me the most frustrating thing is the fact that they have had considerable amounts of good advice and offers of help to resolve these issues but, for what ever reasons, have chosen not to make use of them.
We seem to be getting firmware updates that replace one bug with another, this is hardly moving forward.
Please Seeed and whom ever else is involved in the development of this product start making some real progress or at the very least inform us clearly of your intent so we (I) can either request a refund or have some time scale for a usable product.
Cheers Pete.