BB Green wifi unable to 'login' to setup SSID

Moderators: lily.li, violet, salmanfarisvp, seth.welday

Post Reply
curtis.gunderson
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Jul 11, 2019 8:47 pm

BB Green wifi unable to 'login' to setup SSID

Post by curtis.gunderson » Thu Jul 11, 2019 11:37 pm

Hello - I setup the BeagleBone Green Wireless device through the setup directions. I'm on Win10 and I see the device when connected USB to PC.

I am able to browse to the device as well as use Cloud9 IDE to connect to the device & run sample code to toggle LEDs.

My issue is that when I go to configure WiFi, by connecting my PC wireless or my smart phone to the device's wifi, I see the connect (BeagleBone-B1AE in my case), and it connects. I get a client IP from the device. However -- it does not redirect me to login with SSID so that I can setup the BBGW to be able to connect. At the top, of my client page, there is 'login'. When I click, it gives me error related to 'oauth' or 'err_name_not_resolved'.

I have flashed to the latest image, Debian 9.5 2018-08-30 4GB SD IoT, and have the same issue.

As troubleshooting for standard linux commands, I connect via SSH to the BBGW. I'm able to build a wpa_supplicant.conf file, but when running 'wpa_supplicant -B -i wlan0 -DWext -c /etc/wpa_supplicant.conf' command, I get error 'failed to initialize driver'. I have a green light onboard for the WLAN embedded led.

Any guidance is appreciated.

curtis.gunderson
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Jul 11, 2019 8:47 pm

Re: BB Green wifi unable to 'login' to setup SSID

Post by curtis.gunderson » Fri Jul 12, 2019 11:11 pm

I still have the problem but debugged further. I believe the issue is that the beaglebone.local and 192.168.7.2 IPs are not setup in the oauth.io Domains site. I tried to attached a picture of where someone needs to make changes, but there is an error that the board attachment quota has been reached.

I created my own oauth.io domain app as shown in the picture. Of course, I do not have rights to the ID in the script, N46nTD88b9rs7E-K0FUAqt8JUi0, to make these changes. When I created my app as shown with the 'nK4F...' app keys and the domains shown, GitHub pop-up window will open and prompt me to login. However, since in my app I do NOT know the response urls, it fails.

I think the solution needs to be that the owner of the 'N46nTD88b9rs7E-K0FUAqt8JUi0' app key needs to add beaglebone.local and/or 192.168.7.2 and/or other 6.2/8.2 addresses in oauth.io so that github<>oauth will recognize a valid requester.

Alternatively, if someone can respond with the proper response URL for my github application, I can create my own github project to allow me to continue ( I have a second picture of this, but the github field is found by: click on profile icon > settings > developer settings > oauth apps > {your app} > field 'Authorization callback URL' )

curtis.gunderson
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Thu Jul 11, 2019 8:47 pm

Re: BB Green wifi unable to 'login' to setup SSID

Post by curtis.gunderson » Tue Jul 16, 2019 9:52 pm

I was able to workaround the login/oauth issue, but I still have the problem with not being redirected to the WIFI/SSID login page so that I can configure & save credentials through the app.

When I connect to my 'beaglebone-xxxx' on the bbgw, it gets connected, I get an IP, but it does NOT redirect me to the SSID login page as shown in the user guide. I've tried from multiple devices, I've enabled popups - removed all browser security actually - which is how I discovered the unrelated oauth issue.

Please assist - is there a device url where I can launch the ssid login screen manually - I cannot seem to find it searching the linux directories.

Regarding the oauth issue...the problem is that the oauth credentials are stored in the github_login.js file on line 10. Since I do not own that credential, I cannot login to oauth/github to update the domain to include .7.2/beaglebone.local as authorized sources. The workaround for me was: create my own oauth app, create my own github app, integrate the two (https://coderwall.com/p/sjbwcq/javascri ... -for-oauth )...then, replace the token on line 10 with the own created in the process above. Now, when I refresh, and click the login...I am prompted to login with my credentials to github, where the oauth app is authorized, and i get logged in. However...this is not the wifi connection redirect page.

bill.yu
Junior-6
Junior-6
Posts: 638
Joined: Mon Apr 02, 2018 11:05 am

Re: BB Green wifi unable to 'login' to setup SSID

Post by bill.yu » Thu Jul 25, 2019 1:50 pm

Hi there~

The factory firmware is included the auth page. You can download it from https://drive.google.com/open?id=1fmon- ... znXRFm1UmP.

The latest image does not include the auth page any more. You can refer to https://github.com/Pillar1989/wifidog-server. thanks.

Post Reply