Seeed Github Update: TFT_Touch_Shield_V2 Now fully supports the Seeeduino Cortex M0+ platform.

Grove is a modulated, ready-to-use tool set.
Much like Lego, it takes a building block approach to assembling electronics.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
elaine.wu
Pre-kindergarten
Pre-kindergarten
Posts: 12
Joined: Mon Nov 05, 2018 5:59 pm

Seeed Github Update: TFT_Touch_Shield_V2 Now fully supports the Seeeduino Cortex M0+ platform.

Post by elaine.wu » Thu May 30, 2019 5:31 pm

Github update

TFT_Touch_Shield_V2 Arduino driver library update. Now add the following platform-driven support:
Arduino Uno(all revisions)/Seeeduino(V4&V4.2)
Arduino Mega/Seeeduino Mega
Arduino Zero(M0)/Seeeduino Lorawan
Arduino Leonardo/Seeeduino Lite
Seeeduino Cortex-M0+/Seeeduino Lotus Cortex-M0+
For specific updates, see our update log here.

Image

Grove_LoRa_433MHz_and_915MHz_RF Arduino driver library update. Now we add support for the hardware serial port, and add support for the Cortex M0 platform.

Image

Arduino Uno(all revisions)/Seeeduino(V4&V4.2)
Arduino Mega/Seeeduino Mega
Arduino Zero(M0)/Seeeduino Lorawan
Arduino Leonardo/Seeeduino Lite
Seeeduino Cortex-M0+/Seeeduino Lotus Cortex-M0+

The detailed update log can be checked here. Here is the test result.
Image

bill.yu
Junior-7
Junior-7
Posts: 732
Joined: Mon Apr 02, 2018 11:05 am

Re: Seeed Github Update: TFT_Touch_Shield_V2 Now fully supports the Seeeduino Cortex M0+ platform.

Post by bill.yu » Mon Jun 03, 2019 6:09 pm

thanks for the efforts to make the shields and boards with more compatibility. :D

Post Reply