seeeduino Mega 1.21 Busted Mini USB workaround?

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
skilljohnson
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Dec 30, 2010 7:32 am

seeeduino Mega 1.21 Busted Mini USB workaround?

Post by skilljohnson » Thu Dec 30, 2010 8:08 am

A few months ago the little micro usb connector popped off of my seeeduino mega PCB, and back then I was not very proficient at wielding the $2.99 fire starter that I like to call a soldering iron, so long story short, after a few hours and a lot of cursing I found myself with most of the traces leading from FTDI to usb connector burnt to a crisp, with a tiny little c-hair left, peeking out from under the FTDI obstacle. So I then tried to super glue some wires into position with the tips touching the legs of the chip, to no avail. The 'duino still works, because I can see it running the last sketch that I was able to upload onto it, but I can't get my PC to recognize any arduinos in my USB device list, no matter how vigorously I shake my fist and curse... it's really aggravating, and after having a go with some other MCUs I still yearn for my old, faithful arduino clone back on my cluttered desktop. As previously mentioned, this happened a few months ago, and during that time I posted this same story to a different board, and they said it is possible to bypass the FTDI but I would need to wire up an auto reset circuit or something. Sounds easy enough... if I knew where to begin. So now I am trying one last attempt at getting this thing going again, and any help would be so appreciated, I will dedicate a song to you the next time I sing karaoke.

Just in case it helps, or at the very least provides 12 seconds or so of entertainment, I uploaded a graphical depiction of the injured seeeduino, and I have a couple other MCUs that can transmit/rec data over TTL serial, which should probably help me out, right? I also have a USB-Serial cable, although I don't think it is an 'FTDI' type cable. The only thing close to a description I can offer is that the cable has a ~2" x 3" x .5" or so box shape completely encased in rubber-like-impenetrable plastic. Anyway, thanks in advance for your time and assistance.
Attachments
RIP Duino_lores.jpg
no bueno
RIP Duino_lores.jpg (138.54 KiB) Viewed 2337 times

User avatar
SQX
Kindergarten
Kindergarten
Posts: 52
Joined: Mon Aug 02, 2010 11:13 am

Re: seeeduino Mega 1.21 Busted Mini USB workaround?

Post by SQX » Thu Dec 30, 2010 9:57 am

Hi,

You can bypass the FTDI, you can refer to the following picture that I have to try, and it can program the seeeduino Mega.

Thanks!
Attachments
f8fa979a9d6c155123dc92136df9ed56.image.300x225.jpg
f8fa979a9d6c155123dc92136df9ed56.image.300x225.jpg (74.28 KiB) Viewed 2334 times
---Dare to create and enjoy!

skilljohnson
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Dec 30, 2010 7:32 am

Re: seeeduino Mega 1.21 Busted Mini USB workaround?

Post by skilljohnson » Sun Jan 02, 2011 6:45 am

thank u thank u thank u

Post Reply