Stalker v3.1: Question re: I2C selectable voltage

Arduino, Seeeduino Serials and mutants. Share your problems and experence on arduino compatible board such as seeeduino/stalker, etc.

Moderators: lily.li, violet, salmanfarisvp

Post Reply
pbanders
Pre-kindergarten
Pre-kindergarten
Posts: 11
Joined: Mon Dec 10, 2018 10:48 pm

Stalker v3.1: Question re: I2C selectable voltage

Post by pbanders » Thu Jan 17, 2019 3:50 am

The Seeed product page for the Stalker v3.1 says:

"I2C Pin header (operation voltage is selectable: 5.0V or 3.3V)"

How is the voltage selectable? There's no switch or pad to disable the level shifter? Can this be done or is this spec in error?

User avatar
bestlux
Kindergarten
Kindergarten
Posts: 84
Joined: Wed Jan 30, 2019 11:51 am

Re: Stalker v3.1: Question re: I2C selectable voltage

Post by bestlux » Fri Feb 01, 2019 4:47 pm

Hello,
Do not worry, look at the shifter circuit in schematic there. When you plug in grove of 3.3V or 5V directly, the circuit will match the level automatically.
Image

pbanders
Pre-kindergarten
Pre-kindergarten
Posts: 11
Joined: Mon Dec 10, 2018 10:48 pm

Re: Stalker v3.1: Question re: I2C selectable voltage

Post by pbanders » Sun Feb 03, 2019 6:26 am

Thanks - maybe that's obvious to you that the level shifter handles this automatically, it isn't to me! When I read the VCC pins in the Grove sockets, I see 5V. I don't seem to have any 3.3V Grove devices, so I'll take your word for it. Thanks again for your reply.

User avatar
designnotes.com
Pre-kindergarten
Pre-kindergarten
Posts: 10
Joined: Mon Jan 28, 2019 11:08 pm
Location: Philadelphia, PA
Contact:

Re: Stalker v3.1: Question re: I2C selectable voltage

Post by designnotes.com » Sat Feb 09, 2019 10:39 pm

pbanders wrote:
Thu Jan 17, 2019 3:50 am
The Seeed product page for the Stalker v3.1 says:

"I2C Pin header (operation voltage is selectable: 5.0V or 3.3V)"

How is the voltage selectable? There's no switch or pad to disable the level shifter? Can this be done or is this spec in error?
Hi,

When they say selectable then it means then it will work in the range of this voltage. Like in Arduino it is written that its operating voltage is 7-12 volts it means it works on any voltage in between this range. But it depends on your load if the load is HIGH then your device will not be able to handle that load.


https://store.arduino.cc/usa/arduino-uno-rev3

Post Reply