Support for Ubuntu

Hi guys,



Is there any ubuntu image for respeaker core v2.0 ?

if no, then is there any possibility that ubuntu can be installed in respeaker core v2.0 ? i tried once using ubuntu iot but it can not boot.



Thanks.

Hi there,



We do not have the Ubuntu image this moment. Yes, ubuntu can run on the respeaker core v2.0. we may release a ubuntu image in next release. thanks.



best rgds

Bill

Just want to throw out support for Ubuntu on the Respeaker Core V2. I’m building a robot and the Core V2 works really well with Mycroft and I was able to get ROS (robot operating system) installed on it by building it from source. However, it would have been MUCH easier to do so using Ubuntu since they build packages for that particular flavor (not Debian). All I would have needed to do if it was running Ubuntu is some apt-gets and I’m done. In the end, my installation from source works and the repseaker is the mouth and ears of my robot, but you may have an untapped market (ROS-users) if you could get Ubuntu on it.