It’s the last firmware can loaded to Common hardware of Nano,The FFT & 2M version need a 103VE replaced,so there are no farther Paul version again.
Hardware V1.3 or V1.5 upgrade not recommanded,for the firmware have not been tested .
It’s the last firmware can loaded to Common hardware of Nano,The FFT & 2M version need a 103VE replaced,so there are no farther Paul version again.
Hardware V1.3 or V1.5 upgrade not recommanded,for the firmware have not been tested .
Hi Paul - can you also upload your source code if you can’t continue developing it? Perhaps someone else can continue your excellent work?
Cheers!
Is there an English user guide available for this firmware or perhaps someone using it for a while is willing to share lessons learnt?
Sorry,source code is protected as official designer required.
It’s difficult to me for my poor English,I guess The guy who translated the official guide could do such job too.
Yes, please. I would appreciate a quick guide for the Paul firmware.
SE设置:垂直档位、水平档位、探头倍数,
点按上下,左右实现垂直档位、水平档位调整;
长按上下,左右实现位置调整;
长按M键选择探头倍数;
短按Play启动扫描或暂停扫描 ,
长按Play显示或隐藏所有测量项目.
MO设置:扫描模式、触发模式 ,
按上下选择触发模式,左右选择扫描模式;
短按Play到SE菜单 ,
Tr设置:触发电平、触发灵敏度 ,
按上下调整触发电平,左右调整触发灵敏度。
长按M消隐触发线 ;
短按Play到MO菜单 ,
长按Play直接到SE菜单.
C1设置:十字光标1位置 ,
按上下调整水平光标1,左右调整垂直光标1。
长按M 消隐上次移动的光标上的指示数值–〉消隐上次移动的光标上和指示数值–〉显示上次移动的光标上和指示数值;
短按Play到Tr菜单 ,
长按Play直接到SE菜单.
C2设置:十字光标2位置 ,
按上下调整水平光标2,左右调整垂直光标2。
长按M 消隐上次移动的光标上的指示数值–〉消隐上次移动的光标上和指示数值–〉显示上次移动的光标上和指示数值;
短按Play到C1菜单 ,
长按Play直接到SE菜单.
Me选择:测量模式、设置测量显示模式 ,
按上下选择测量内容,
长按右键显示所有测量项目,
长按左键隐藏;
短按Play到C2菜单 ,
长按Play直接到SE菜单.
Of设置:x轴偏移、y轴偏移 ,
按上下调整垂直偏移,左右调整水平偏移。
长按M消隐水平偏移参考线 ;
短按Play到Me菜单 ,
长按Play直接到SE菜单.
Fo设置:输出脉冲频率 ,
短按上下调整输出脉冲频率档位,长按上下调整输出占宽比;
短按左右细调输出脉冲频率,长按左右粗调输出脉冲频率;
短按Play到Of菜单 ,
长按Play直接到SE菜单.
FL: 文件操作 ,
按右键选择保存,按左键选择读取,按上下选择程序号,长按M执行选择的操作;
长按上下按钮,参考波形位置移动,
长按左按钮,隐藏参考波形,
长按右按钮,显示参考波形.
短按Play到Fo菜单 ,
长按Play直接到SE菜单.
长时间不操作,自动回SE菜单。
参数保存方法:设置好以后至少保证开机5分钟,或者可以在非SE菜单下长按PLAY键直至出现提示;
按住M键开机,可以使用默认的设置。
两时间游标间时间增量转化为频率显示功能:在C1或C2菜单下点按上下按键可在显示时间、显示频率、
自动交替三种模式间切换。
电压校正使用方法:
a)零位校正
按住左键开机,短接探头,打开测量显示。短按上下按钮选择校正的档位,短按左或
右键至显示的平均电压最接近0V。
b)增益校正
准备一个基准电源,按住右键开机,探头接基准电源,打开测量显示。短按上下按钮选择
校正的档位,短按左或右键至显示的平均电压最接近基准电源值。
为取得最好的效果,可重复几次上述过程,完成后短按M键一次,再长按play键保存。如按住M键
开机,将不使用保存的校正数据。
为避免USB充电时示波器显示缓慢,正常开机将屏蔽USB通讯,此时PC会显示不能识别的USB设备,
要使用USB通讯,请按住M键开机。
按住Play键开机,则Play键功能同V1.4版。
^ Google translation from Chinese
Paul’s Firmware 1.5 operation manual.
Translated by Eric Pan from Seeed Studio 5/31/2010
Basic operation:
Press M to switch cycle downwards around menu items.
Press R/S to switch cycle upwards around menu items.
Press R/S and hold to jump back to Se (basic measurement) menu.
Use direction keys to adjust.
After long time idle, firmware jumps back to Se menu
Save parameter:
Keep power for 5 minutes for latest setup, or press and hold R/S button for menu other than Se.
Press M while powering up to use factory setting.
Frequency/Time measurement change.
Press UP/DOWN under C1 or C2 menu to toggle among Time/Frequency/Auto switch
Calibration
a) Zero calibration
Press LEFT while powering up, connect black and red probe. In Se menu, Press UP/DOWN to choose scale needs calibration, press LEFT/RIGHT to adjust the displayed average voltage to 0V.
b) Gain calibration
Prepare a reference power source, press RIGHT while powering up, attach probe to reference power supply. In Se menu, press UP/DOWN to choose the scale needs calibration, press LEFT/RIGHT to adjust the displayed average voltage to the power source.
To get the best result, please repeat above processes, press M after completion, then press and hold R/S to save to parameter.
USB communication
When connected to PC, USB communication is disabled by default, PC will report unrecognizable USB device.
To use USB communication, please press M while powering up.
================================Menu operations as below======================
Se Menu:
To set vertical Scale, Time Base, Probe attenuation scale
Press UP/DOWN to adjust vertical scale, Press LEFT/RIGHT to adjust time base
Press and Hold directions to adjust waveform positions
Press M to switch probe attenuation scale
Press R/S to run and stop waveform
Press and hold R/S to display or hide all measurement items.
Mo Menu:
To set scan mode and trigger mode
Press UP/DOWN to choose trigger mode, Press LEFT/RIGHT to choose scan mode
Tr Menu:
To set trigger level and trigger sensitivity
Press UP/DOWN to adjust trigger level, LEFT/RIGHT to adjust trigger sensitivity
Press and hold M to display/hide trigger level marker
C1 Menu:
To set cross cursor 1 (Red dotted lines)
Press UP/DOWN to adjust horizontal cursor 1, Press LEFT/RIGHT to adjust vertical cursor
Press and hold M to toggle display of latest modified cursor and value
C2 Menu:
To set cross cursor 2 (Blue dotted lines)
Press UP/DOWN to adjust horizontal cursor 1, Press LEFT/RIGHT to adjust vertical cursor
Press and hold M to toggle display of latest modified cursor and value
Me Menu:
To set measurement mode and display
Press UP/DOWN to set measurement mode
Press and hold RIGHT to display all measurement items
Press and hold LEFT to hide
Of Menu:
To set horizontal position and vertical position
Press UP/DOWN to adjust vertical position, Press LEFT/RIGHT to adjust horizontal position
Press and hold M to toggle display of horizontal indicator
Fo Menu:
To set output waveform characteristics
Press and hold UP/DOWN to adjust duty cycle
Press UP/DOWN to adjust frequency in rough stages
Press LEFT/RIGHT to tune frequency in 1% scale
Press and hold LEFT/RIGHT to tune in 10% scale
FL Menu:
To operate file on SD card
Press RIGHT to save, Press LEFT to load, Press UP/Down to select #, Press and hold M to execute.
Press and hold UP/DOWN to move reference form
Press and hold LEFT to hide reference waveform
Press and hold RIGHT to display reference waveform
Tried to translate here. Please let me know if anything mistaken. thanks!
Excellent!
I think the above post is worthy of a PDF available for download from the repository (perhaps even an editable word source so others can add to it).
I still have a couple open questions :
Don’t know about anybody else but I’m having trouble changing the vertical scale using the “up” button in “Se” mode. I can move the waveform up and down by holding it as described, but just pressing up doesn’t reduce the volts/division.
Edit: I’ve got hardware v1.1.
Edit 2: The “up” button needs pressed several times in any mode to register it. Is it polled or does it use an interrupt?
Maybe something jamming the up button?
Thank you, Paul! Very good. The DSO becomes better.
Paul, your firmware is the best, but you can include LOGOS to reeplace seedstudio, dso nano… originally my DSO shows e-design. when I try some firmwares I lost it.
entusiast about this project, i’ve made a brief discussion on it and a manuals’ italian translation
davidea.it/elettronica/45-va … o-201.html
i’m not a professional translator, then if someone find error , please tell me!
piccola recensione e traduzione italiana del manuale, liberamente utilizzabile da chiunque! segnalatemi eventuali errori ed inesattezze.
Hi guys!
I want to share my experience with the DSO nano here.
Just a two days ago I have received one from ebay. It was flashed with the latest Paul 1.5.20 firmware. So everything was ok but the voltage readings was biased with +800mV.
Seeed firmware has no gain and zero adjustments. Paul`s one wont write to microSD its settings.
The 2nd way was more clear so I have started my little research.
Here`s the results.
To have an opportunity of using the microSD card with Paul 1.5 do the following step-by-step:
1- Get an microSD 2GB card (do NOT buy Kingston!). I have Apacer 2GB working good. Maybe you should switch between several vendors.
2- Put the card into the card-reader or notebook and format it in FAT (FAT16) with standard cluster size.
3- Put it in the DSO Nano
4- power the DSO up while holding the M button. Do NOT use any DSO functions to not ruin the microSD filesystem!
5- connect the DSO with the PC with USB cable
6- windows users should check up “my computer” for new removable drive appeared.
6.1-If the new drive have appeared but you see window ‘hang up’ and too sloooow - this microSD card is inappropriate for your DSO. Return it to shop, get another one and repeat from step 1.
6.2-If windows says ‘disk is unformatted - format now?’ - its OK! Click YES, then select type FAT and do full (not quick) format of the flash card.
6.3- maybe you even see an empty disk - so you even dont have to format it.
7 - So you have seen a new drive and can access it from your PC. Pick up the archive DSO.zip attached below and extract files from it to the root folder of your microSD. Take a close attention: their names must contain small letters ONLY (i.e. config.dat not CONFIG.DAT). If not - simply rename it.
8. After all just cycle the power.If you see the mV values instead of Freq and Hz in the quick measure tab and the horizontal cursors are 0V and 5V - you are having success!
DSO.zip (1.01 KB)
Special for those who have no usable SD,but ref wave is limmited to 4,
also worked for those who have an usable SD.
1.6.rar (33.3 KB)
Hi Paul
Thanks - I have just tried your version 1.6, but still get the “File Not Exist” error when I try to save or load waveforms.
Ah - just realised it works if you now remove the SD card! - you are now presumably saving to the ARM memory.
I tried reading this from the USB, but I cannot see it because it is unformatted, even though my Mac reports the presence of the STM-32 mass storage. Any suggestions about how to transfer waveforms to my Mac? - I eventually want to print direct to a Polaroid POGO printer.
Tony
Sorry,there is no way to transfer waveforms to Mac for wave data has been stored in STM flash without a FAT formatted.
And get a usable SD is recommanded because the poor endurance of STM flash .
Hi Paul
Thanks for the advice. So I must return to my other active thread (microSD error) hoping someone will answer why neither of my two SanDIsk 2GB cards will work with the waveform storage but behave OK when the NANO is used as a USB card reader.
If you have any special software I can upload to investigate the problem, please let me know.
Thanks
Tony