Firmware 1.5
Moderators: lily.li, violet, salmanfarisvp, jeremy882, crail.lyu969
Re: Firmware 1.5
1.5! Thanks Paul!
Your firmware was the hottest for DSO nano, excited to see it's updating again! Great work!
Added into google code repository. http://code.google.com/p/dsonano/downloads/list

Your firmware was the hottest for DSO nano, excited to see it's updating again! Great work!
Added into google code repository. http://code.google.com/p/dsonano/downloads/list
Re: Firmware 1.5
Just prepared a firmware upgrade step by step guide, for people who wants to try:
http://code.google.com/p/dsonano/downlo ... f&can=2&q=
http://code.google.com/p/dsonano/downlo ... f&can=2&q=
Re: Firmware 1.5
It's the last firmware can loaded to Common hardware of Nano,The FFT & 2M version need a 103VE replaced,so there are no farther Paul version again.
Hardware V1.3 or V1.5 upgrade not recommanded,for the firmware have not been tested .
Hardware V1.3 or V1.5 upgrade not recommanded,for the firmware have not been tested .
-
- Pre-kindergarten
- Posts: 17
- Joined: Mon Feb 08, 2010 3:47 am
Re: Firmware 1.5
Hi Paul - can you also upload your source code if you can't continue developing it? Perhaps someone else can continue your excellent work?
Cheers!
Cheers!
Re: Firmware 1.5
Is there an English user guide available for this firmware or perhaps someone using it for a while is willing to share lessons learnt?
Re: Firmware 1.5
Sorry,source code is protected as official designer required.peterjohnston wrote:Hi Paul - can you also upload your source code if you can't continue developing it? Perhaps someone else can continue your excellent work?
Cheers!
Re: Firmware 1.5
It's difficult to me for my poor English,I guess The guy who translated the official guide could do such job too.BenF wrote:Is there an English user guide available for this firmware or perhaps someone using it for a while is willing to share lessons learnt?
Re: Firmware 1.5
Yes, please. I would appreciate a quick guide for the Paul firmware.BenF wrote:Is there an English user guide available for this firmware or perhaps someone using it for a while is willing to share lessons learnt?
Re: Firmware 1.5

SE设置:垂直档位、水平档位、探头倍数,
点按上下,左右实现垂直档位、水平档位调整;
长按上下,左右实现位置调整;
长按M键选择探头倍数;
短按Play启动扫描或暂停扫描 ,
长按Play显示或隐藏所有测量项目.
MO设置:扫描模式、触发模式 ,
按上下选择触发模式,左右选择扫描模式;
短按Play到SE菜单 ,
Tr设置:触发电平、触发灵敏度 ,
按上下调整触发电平,左右调整触发灵敏度。
长按M消隐触发线 ;
短按Play到MO菜单 ,
长按Play直接到SE菜单.
C1设置:十字光标1位置 ,
按上下调整水平光标1,左右调整垂直光标1。
长按M 消隐上次移动的光标上的指示数值--〉消隐上次移动的光标上和指示数值--〉显示上次移动的光标上和指示数值;
短按Play到Tr菜单 ,
长按Play直接到SE菜单.
C2设置:十字光标2位置 ,
按上下调整水平光标2,左右调整垂直光标2。
长按M 消隐上次移动的光标上的指示数值--〉消隐上次移动的光标上和指示数值--〉显示上次移动的光标上和指示数值;
短按Play到C1菜单 ,
长按Play直接到SE菜单.
Me选择:测量模式、设置测量显示模式 ,
按上下选择测量内容,
长按右键显示所有测量项目,
长按左键隐藏;
短按Play到C2菜单 ,
长按Play直接到SE菜单.
Of设置:x轴偏移、y轴偏移 ,
按上下调整垂直偏移,左右调整水平偏移。
长按M消隐水平偏移参考线 ;
短按Play到Me菜单 ,
长按Play直接到SE菜单.
Fo设置:输出脉冲频率 ,
短按上下调整输出脉冲频率档位,长按上下调整输出占宽比;
短按左右细调输出脉冲频率,长按左右粗调输出脉冲频率;
短按Play到Of菜单 ,
长按Play直接到SE菜单.
FL: 文件操作 ,
按右键选择保存,按左键选择读取,按上下选择程序号,长按M执行选择的操作;
长按上下按钮,参考波形位置移动,
长按左按钮,隐藏参考波形,
长按右按钮,显示参考波形.
短按Play到Fo菜单 ,
长按Play直接到SE菜单.
长时间不操作,自动回SE菜单。
参数保存方法:设置好以后至少保证开机5分钟,或者可以在非SE菜单下长按PLAY键直至出现提示;
按住M键开机,可以使用默认的设置。
两时间游标间时间增量转化为频率显示功能:在C1或C2菜单下点按上下按键可在显示时间、显示频率、
自动交替三种模式间切换。
电压校正使用方法:
a)零位校正
按住左键开机,短接探头,打开测量显示。短按上下按钮选择校正的档位,短按左或
右键至显示的平均电压最接近0V。
b)增益校正
准备一个基准电源,按住右键开机,探头接基准电源,打开测量显示。短按上下按钮选择
校正的档位,短按左或右键至显示的平均电压最接近基准电源值。
为取得最好的效果,可重复几次上述过程,完成后短按M键一次,再长按play键保存。如按住M键
开机,将不使用保存的校正数据。
为避免USB充电时示波器显示缓慢,正常开机将屏蔽USB通讯,此时PC会显示不能识别的USB设备,
要使用USB通讯,请按住M键开机。
按住Play键开机,则Play键功能同V1.4版。