linkit7688 file system corruption and libmraa

Moderators: lily.li, violet, salmanfarisvp

Post Reply
andrew.mcmeikan
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Thu Aug 02, 2018 9:58 am

linkit7688 file system corruption and libmraa

Post by andrew.mcmeikan » Thu Aug 02, 2018 10:13 am

HI All,
Having developed code and designed a commercial product using dozens of embedded linkits, I am facing a problem where the file system corrupts.

Lots of 0 byte random files start appearing and eventually will not boot.

I am using v0.8.2 boot loader and V0.9.4 firmware (kernel 3.18.23), my application is in c and uses libmraa for fast (~1MHz) I/O control.

I have added hardware that powers off when I halt (as reboot clear I/O).

The corruption occurs with or without running off an SD card.

I have attempted to migrate to using LEDE, but it does not seem possible to get libmraa working as there seems to be version incompatibilities.

I am hoping someone has solved these problems

I am also chasing full source code (i.e. including the source for the libmraa that comes with the board)

Thanks in advance.

Andrew McMeikan

bill.yu
Junior-6
Junior-6
Posts: 644
Joined: Mon Apr 02, 2018 11:05 am

Re: linkit7688 file system corruption and libmraa

Post by bill.yu » Fri Aug 03, 2018 9:52 am

Hi there,

Please try to submit a post on https://en.forum.labs.mediatek.com/c/linkit-smart-7688. the mediatek will answer the questions. thanks.

Bill

Post Reply