I’m afraid I have not been able to duplicate this, tried various timebases, trigger types, etc. Might help if you describe in detail exact settings used such as timebase, trigger types, trigger levels (try auto trigger), any other functions active at the time such as trigger delay, decode modes, etc, as well as which channel you are turning the source signal on/off. Does this only happen when you FIRST engage A&B mode? After you re-engage can you still reproduce the issue by shutting off the source?
One possibility with V5.1 behaving like this could be memory allocation issues like the one when this version was loaded on HW 2.81. When loaded on earlier devices, for some reason the problems did not seem to exist, but it was not clear to me at the time why this was so. Odd triggering issues like this were typical with V5.1 loaded on HW 2.81. After working on the upcoming update (V5.2/V6.1) the same memory issues started creeping up on early devices. These have now been resolved, am in the process of finishing a chart mode update, and will be posting this shortly. If I don’t find anything else in the meantime, I would suggest trying the next update to see if it fixes the problem.
V3.4 however did not have any memory allocation issues, so if this existed in that version, would point to something else, also tried another older device with the original V5.1 loaded and still could not duplicate this. Finally, you could try resetting the configuration by removing the WPT file (save it so you can return it to the device afterwards), corrupted config files can sometimes cause strange behavior.
thanks for your quick reply. After reading your words, I suspect that I might have a hardware problem. After investigating a bit further, I was able to break it down to the use of “NORML” trigger mode, as I usually leave it to “AUTO” and it gets switched to “NORML” in A&B mode, just as stated in your manual.
Attached my used config file and four screenshots, where I used “NOISE” as signal input (in real life I came across this while measuring PWM signals). It has been the same in wc3.4 and wc5.1 (factory app doesn’t support A&B mode, so I cannot test with that). In all screenshots the signal generator was connected to both channels. “NOISE” I only used because it’s directly next to “OFF”, the problem persists with any signal form.
When switching from TR D (rising edge) to A&B, channel A is dead most times (nearly always)
When switching from TR A (rising edge) to A&B, channel B is dead (sometimes)
When cutting input signal while in A&B (rising edge) and activating signal again, both channels are dead (most times)
Seldomly I am able to display both signals in A&B mode, but sometimes this is the case (see IMAG007.bmp, but it took about 10 tries to achieve this).
In AUTO mode, there’s absolutely no problem. Also, as long as the signal isn’t cut off, it doesn’t freeze once it works.
Possible causes I currently see:
my device has a hardware fault that leads to faulty triggering in NORM mode
my config file is corrupt
it’s normal for this mode, and I misunderstand the concept behind this
Please don’t investigate too much, as I see it as a minor bug (in fact I accidentially activated A&B mode in wc3.4 and wondered why my channel suddenly seemed dead, mostly I use AUTO trigger mode for single channel). Unfortunately I have no option to test a different DSO203, as I only have this one available.
Looking at your screenshots, I can see why you are getting these results, at least with the waveforms you are displaying:
You are using the auto trigger mode on a wave with a significant DC offset while in DC coupling mode. This pushes the waveform up away from the baseline. When not triggered, the auto trigger function looks for crossing events at the baseline, so it doesn’t “see” the wave riding on the DC offset above, unless it catches some transient while switching functions. Once triggered, it depends on the displayed waveform to establish a mid-point reference but in normal mode, no signal is displayed until it is triggered, unlike in auto mode.
The obvious solution is simply to shift the coupling mode over to AC. Notice that ALL outputs from the internal generator have this DC offset.
Another solution, if the DC offsets are desired to be displayed in DC coupling mode, is once triggering level is established with AUTO trig and waveforms are properly triggered, freeze the setting by long pressing button 2, this shifts over to manual mode. Or just simply move the trig cursor to the proper level in manual mode. When manually shifting the trigger level in A&B mode, both channels move together, so it may be necessary to shift triggering source to one or the other channel to set that level, then shifting back to A&B mode.
Setting auto trig with a short press of button 2, then following with a long press to freeze the setting is a sequence I use extensively with these devices, since auto trig can cause the trig level to fling around a lot in trying to follow rapidly changing waveforms.
I see, the problem was that I misunderstood the concept, and there’s no system fault at all. Using manual trigger level truly solved the problem for me.
For me it is absolutely desirable to display pulsating DC “as is”, as currently I mainly measure PPM and PWM signals in lipo powered model flight hardware (that’s why I chose a pocket device that I can use at the flying fields) and the like and need to see the true voltages next to pulse width and frequency, so AC coupling is not a solution for me.
Many thanks for your efforts and pointing me to the right direction. Again have learned something!
Mainly updates CHART mode to fix improper ADC operation at slowest timebases. Changed chart buffer to oversampling and added selection of either averaging or oversampling (peak hold) modes. Select while in chart mode with menu on timebase adjust, short press left toggle center to access chart mode auto file write, press again to access buffer mode. Change with left toggle. Defaults to averaging but selection is saved with config files.
FPGA based OS function proved to be not well suited for slow chart operation, so used software instead. Since this does not depend on FPGA hardware, the revised chart mode is compatible with older versions as well and so is also included in V5.2
Oversampling factors vary from 100X at 0.1S/div to 600X at 10Min/div. eg: at 10Min/div, the device obtains 30 readings per second for a total of 600 during the 20 second span for each the 30 steps in one division (600sec/30steps), then either averages them to produce one sample or stores the + and - peaks for display. Averaging will reduce noise while oversampling captures any noise or signal spikes.
Other fixes: (See readme.txt for more info):
V6.1:
-Fixed long buffer mode not always initiating when recalled from a config under some conditions.
Also forgot to include the W1.1 FPGA code in V6.1 (Required, if not already installed from previous update, to use full speed oversampling mode on hardware V2.81 and up ONLY)
Thanks Wildcat again for the updates.
I've asked MiniDSO for details about HW v2.82 this is what i've got:
"HW2.82 is only a small part of the layout is different, the same hardware"
I also asked about DFU v3.46C and got they said it is HW2.81 compatible. They also provided the rom to flash the STM like i requested:
http://www.minidso.com/forum.php?mod=viewthread&tid=1202&extra=page%3D1
I have now updated to DFU v3.46C from v3.45C and here's the funny part:
Before as you know on my main intel i7 win10 laptop when copying your application it would disconnect the DFU drive while copying making it impossible to install your application. (smaller files like FPGA are able to installed normally)
That's why i've used and old winxp desktop machine which worked fine because it will copy the files without disconnecting the DFU drive.
A week or so ago i installed your v6.1 when it was running DFU v3.45C with that winxp system.
Today i updated to DFU v3.46C and while the app1.hex copies fine like expected, it will always give .ERR and the application will not install. I've tried different versions and stuff, always giving the same .ERR on app files, but then i went to my brother's core duo laptop running win10, and guess what? It installed it without an issue.
I got this idea because i saw a post with someone with a hw v2.82 having the same issue here, and he made a thread over minidso forums, saying he successfully installed your app on a win10 machine.
So from what i understand they managed to f**k up DFU even more that before. What do you recommend to do with this issue since more people are having this type of incompatibility with different systems. I suggest that i make a thread over minidso to get their attention hopefully to get it fixed with a newer DFU update. What do you think? You might say update is difficult but with a cheap USB to RS232 adapter and the tutorial i made it is very easy for anyone.
I wouldn’t be too hard on the factory guys, Microsoft likely changed, on purpose just to screw things up, the way these (to them obsolete) volumes are accessed in their new Windows versions.
It would seem though there should be some way the DFU could probe the host system to find out what version of Windows is accessing it, then readjust itself accordingly. Or simply have a menu so the user can select the proper Windows version.
Not sure though how many users are willing to open their devices, solder some pins and attach a serial connection to their PC in order to do this. On a bricked unit, yes, but on a perfectly good device it seems much simpler (and safer) to just find an older computer to upgrade with.
DFU always has been kind of funny. I once had a problem (not with wildcat, but with gabonator) reinstalling: always got an .err. Needed to reinstall because by accident I overwrote part of the code. Solution was: install something completely different into the same slot, and then try again. Which in fact solved the problem!
Was not Win10 though, but Win XP (my older 2.70 device with DFU 3.11C). So in case reinstalling whatever doesn’t work, one could possibly succeed by following that procedure.
Yes i get your point, but it is really weird that only this specific device has such an incompatibility problem, where you saw it doesn’t seem to be OS specific but rather than system specific. Also it will still affect new devices sold to customers, and i think they might not being even aware of this issue. I thing i should just make a thread to see what they have to say about it at least
Yes i was thinking to do something like this but couldn’t find the original app on that (winxp) system so i happened to try the other win10 system and it worked. If i remember i will try this next time to see if it makes a change or not Another thing worth noting though, it actually required me to re-install the fpga after installing wildcat on that win10 system, where i had already installed it multiple time successfully on the winxp system multiple times. What’s up with that?
The DFU update you downloaded from the MiniDSO site is a complete ROM update, including the V1.64 Sys and the original FPGA and LOGO, along with their APP, that’s why the FPGA reverted to the original.
Yes that’s correct, i know this, that’s why i installed your FPGA first before attempting to install the APP. However after successfully installing your APP i needed to re-install the FPGA again even though i installed it successfully. I know it sounds weird because it is.
Is there a way to rename saved configs and display custom titles for the configs on the screen?
I have 9 or 10 different config files set up, each tuned to handle a different task, but it can be quite difficult remembering which config is for which task. I’ve used a sticky-note to keep track but I change these configs enough sometimes that it’s easy to get confused or lose track of these configs.
But it would be great if I could rename these config files to something else in order to get a better idea of what they’re for.
Would require a rather extensive rewrite and expansion of the config file access function. I agree it would be a nice touch. Memory is getting pretty low though, specially with the older devices. Will keep it in mind.
With regards to other suggestions made, one was automatic saving of config files: gave this some thought, one problem is that this would disrupt the display for a second or two while saving, so if done often enough on a time basis to be effective, could become annoying as well as result in lost data. Likewise if done after menu changes: It would have to be continually saving configs after changing settings to be effective enough to save the last configuration. Otherwise, when would you have the config save itself?
As far as a past suggestion to change the shortcuts, I’m reluctant to do this. I suspect most users are by now familiar with the operation as it is, changing things would likely lead to frustration.
Great job on the latest update (v6.1). I really like Chart Mode now.
On suggestions for added features…
It would be really nice to have a DC offset feature on CHA and CHB. This would allow adding or subtracting a fixed value of vertical offset in DC mode. This is a feature provided on more advanced oscilloscopes and allows observation of small variations of signals with large DC offsets. There is a hardware work around by using channel C’s A-B mode and external adjustable DC source. Alternatively switching AC coupling on removes DC bias, but there can be reasons for wanting to see the DC bias along with the signal.
The hardware is not designed to be able to do this. The only software access to the signal path is at the output of the preamp, at the unity gain inverter that drives the ADC, so while you can shift the wave up/down, any DC applied to the input beyond one screen’s height will clip at the top just the same, so if you shift the wave down you will just see the clipped signal.
This has already been observed with some devices that clipped at a lower level than the top of the screen, and required the ADC “window” shifted down to hide the clipping.
Likewise, using ChD’s A-B mode with what I presume you mean is a DC signal on the B channel balancing the wave on ChA, if DC on ChA is large enough it will still still clip the waveform at the same level (roughly at the top of the screen), even though it may appear at a lower position. The A-B mode is mixed by the software, after the ADC has processed the signal, so it has no real effect on either ChA or ChB’s DC offsets.
To work properly, DC compensation for this purpose needs to be done at the input, so that the preamp doesn’t “see” it, and there is no provision for this in the device. Otherwise the very small dynamic range of these devices, limited to just about one screen’s height will just not allow it.
This is a compromise that must be made to keep power consumption down when running on batteries, voltage levels must be kept low, limiting dynamic range.
I guess a hardware circuit could be how those advanced scopes are handling the DC offset function.
Is it possible to set the ADC’s upper and lower reference voltages? I was thinking you might be able raise the lower reference voltage while still keeping the higher reference voltage above the signal level.
This excellent youtube.com video doesn’t discuss clipping, but explains the usage of oscilloscope offset function with DC offset waveforms.