OK, first screen is on battery with sleep timer off, second is on charger. In both cases readings drop down long before first line of the grid (10min).
Can I ask you to try this setup with your device? A simple Li-Po battery or other DC source, connected to probes with 10min timebase.
Ok, when I first looked at your first screenshots, I thought the problem was that the level was dropping down to 0 after ~ 10 mins, I didn’t notice the cursor on top indicating this was just as far as the readings had advanced, that’s why I suggested the standby timer. So the problem is the drop down to around 1/2 level.
I just let one of my devices run at 10M/div with these settings for around 40 mins, and although I didn’t get any drop in level, when first started the level was wrong, at about this 1/2 level, as if perhaps the range hadn’t been updated properly. After shifting the timebase to a faster position, it corrected itself. This may be related to what you are experiencing.
I will check this over to see what’s going on… I need to know what versions you are using. Presumably, since you loaded V6.0 of the program you have hardware 2.81, I need to verify this. I also need to know what FPGA version you are using, factory, V1.0 as included in the APP 5.0 or V1.1 included in APPS 5.1 and 6.0.
First one is taken after purchase of the device, no mods. Second is with latest WC6.0. FPGA is from 6.0. Before that there was 5.1 with FPGA from it, same problem. Never tried 5.0.
I bought a brand new DSO203: Hardware 2.82, SYS Ver 1.64, Serial No 792BD89A).
I tried to install Wildcat Version 5.1 => but uploading app1.hex via DFU results in app1.err.
So I uploaded FPGA_281.ADR, 281_FPGA.BIN and app1.hex (all Wildcat 5.1)=> uploading is perfectly done => but restarting dso hangs in splash screen showing “FGPA configuration error”
After that I tried these configurations without success:
Thanks for the feedback. I have used the chart mode extensively, but always at the faster timebases, so never noticed these issues. Checking all possible combinations of the different functions on this program is rather time consuming, I rely on feedback from users to pick up on what I may have missed.
Did a fair amount of checking over the software and running tests on this, it appears that the ADC simply doesn’t work reliably when clocked at speeds of less than 1Hz or so. (clock rate at the 10Min/div TB is 1/20Hz). This is not too surprising, given that the minimum recommended signal to noise based conversion speed rating of the ADC is 1Mhz! Nonetheless, all ADC versions seem to work well at 30Hz (1Sec/div). I suspect the limitation here is in the sample/track and hold front end in the ADC chip, which under these conditions is asked to hold much longer than it was designed.
The “glitches” in your first screenshot may also have been caused by this. I have a different version ADC in mine, which could explain the somewhat different results.
The way to fix this is to oversample the chart mode (presently the regular OS functions are disabled in this mode). The hardware is already setup for this in V2.81 when used with the FPGA that comes with 5.1/6.0 so it should be possible to get around the problem by raising the clock speed this way. This would also improve on signal acquisition, since many more samples would be taken. Averaging and peak holding could also then be selectable , as in the regular timebases.
Unfortunately, for devices prior to HW 2.81, the factory FPGA that comes with these doesn’t support oversampling, and since the FPGA chips in those are from a different manufacturer (now out of business) I cannot reprogram them. The range on these older devices may have to be restricted to speeds that work reliably.
EDIT: hardware (FPGA) OS functions have proven not well suited for slow chart speeds, so a software function was developed instead. This will also be included in 5.x versions for older devices.
Will be working on this as time permits, and post an update once a fix is implemented.
I have no way of verifying operation on devices other than up to 2.81, neither can I find any info on HW 2.82
Some suggestions:
-Older versions of Windows (XP, 7) seem to be more reliable for upgrading. What is the DFU version ? (shows on screen when updating). Later versions of Windows are fussy as to which version the DFU is. Also it’s been reported that turning on the device before plugging in the USB is more reliable on later Win versions.
-A directory on your PC screen shows both app1 and FPGA being updated. I have always updated the APP and FPGA separately, shutting off the device and re-connecting the USB in between. It appears that you updated BOTH APP and FPGA at the same time. I don’t know if there is a problem in doing this, I have just never tried it. You may want to try just uploading the APP hex file, then disconnecting and then starting over again and upload the ADR file, wait for the volume to reappear then copying the FPGA BIN file.
-Use Wildcat version 6.0 rather than 5.0 or 5.1, there have been some issues with versions 5 when used on HW2.81.
I realize you have HW2.82, but it looks like your problem was initiated using Windows File Explorer in Win XP to install WC FPGA1.1. Is this correct?
I had just the opposite experience with HW2.81. My SYS was corrupted by using Window 10 to install WC’s FPGA1.0.bin in DFU mode (DFU 3.45C), then restored using Windows XP.
Before I got trouble with “fpga configuration error”, I had tried to upload firmware wc4.4, 5.1 and 6.0. Uploading app1.hex always resulted in app1.err. Therefore I tried the stuff with a new FPGA upload.
BUT!!
I have an additional DSO 203 which had smoked on short circuit against mass. :x
That DSO was HW 2.81. Ugrading to WC4.4 simply had needed to copy app1.hex. I had used the same XP machine.
I’m afraid I have not been able to duplicate this, tried various timebases, trigger types, etc. Might help if you describe in detail exact settings used such as timebase, trigger types, trigger levels (try auto trigger), any other functions active at the time such as trigger delay, decode modes, etc, as well as which channel you are turning the source signal on/off. Does this only happen when you FIRST engage A&B mode? After you re-engage can you still reproduce the issue by shutting off the source?
One possibility with V5.1 behaving like this could be memory allocation issues like the one when this version was loaded on HW 2.81. When loaded on earlier devices, for some reason the problems did not seem to exist, but it was not clear to me at the time why this was so. Odd triggering issues like this were typical with V5.1 loaded on HW 2.81. After working on the upcoming update (V5.2/V6.1) the same memory issues started creeping up on early devices. These have now been resolved, am in the process of finishing a chart mode update, and will be posting this shortly. If I don’t find anything else in the meantime, I would suggest trying the next update to see if it fixes the problem.
V3.4 however did not have any memory allocation issues, so if this existed in that version, would point to something else, also tried another older device with the original V5.1 loaded and still could not duplicate this. Finally, you could try resetting the configuration by removing the WPT file (save it so you can return it to the device afterwards), corrupted config files can sometimes cause strange behavior.
thanks for your quick reply. After reading your words, I suspect that I might have a hardware problem. After investigating a bit further, I was able to break it down to the use of “NORML” trigger mode, as I usually leave it to “AUTO” and it gets switched to “NORML” in A&B mode, just as stated in your manual.
Attached my used config file and four screenshots, where I used “NOISE” as signal input (in real life I came across this while measuring PWM signals). It has been the same in wc3.4 and wc5.1 (factory app doesn’t support A&B mode, so I cannot test with that). In all screenshots the signal generator was connected to both channels. “NOISE” I only used because it’s directly next to “OFF”, the problem persists with any signal form.
When switching from TR D (rising edge) to A&B, channel A is dead most times (nearly always)
When switching from TR A (rising edge) to A&B, channel B is dead (sometimes)
When cutting input signal while in A&B (rising edge) and activating signal again, both channels are dead (most times)
Seldomly I am able to display both signals in A&B mode, but sometimes this is the case (see IMAG007.bmp, but it took about 10 tries to achieve this).
In AUTO mode, there’s absolutely no problem. Also, as long as the signal isn’t cut off, it doesn’t freeze once it works.
Possible causes I currently see:
my device has a hardware fault that leads to faulty triggering in NORM mode
my config file is corrupt
it’s normal for this mode, and I misunderstand the concept behind this
Please don’t investigate too much, as I see it as a minor bug (in fact I accidentially activated A&B mode in wc3.4 and wondered why my channel suddenly seemed dead, mostly I use AUTO trigger mode for single channel). Unfortunately I have no option to test a different DSO203, as I only have this one available.
Looking at your screenshots, I can see why you are getting these results, at least with the waveforms you are displaying:
You are using the auto trigger mode on a wave with a significant DC offset while in DC coupling mode. This pushes the waveform up away from the baseline. When not triggered, the auto trigger function looks for crossing events at the baseline, so it doesn’t “see” the wave riding on the DC offset above, unless it catches some transient while switching functions. Once triggered, it depends on the displayed waveform to establish a mid-point reference but in normal mode, no signal is displayed until it is triggered, unlike in auto mode.
The obvious solution is simply to shift the coupling mode over to AC. Notice that ALL outputs from the internal generator have this DC offset.
Another solution, if the DC offsets are desired to be displayed in DC coupling mode, is once triggering level is established with AUTO trig and waveforms are properly triggered, freeze the setting by long pressing button 2, this shifts over to manual mode. Or just simply move the trig cursor to the proper level in manual mode. When manually shifting the trigger level in A&B mode, both channels move together, so it may be necessary to shift triggering source to one or the other channel to set that level, then shifting back to A&B mode.
Setting auto trig with a short press of button 2, then following with a long press to freeze the setting is a sequence I use extensively with these devices, since auto trig can cause the trig level to fling around a lot in trying to follow rapidly changing waveforms.