Xadow Edison Mainboard battery connector

Is there a BOM of the Xadow Edison Mainboard available? Or does someone know the exact type of the battery connector used?

Hello,

JST 1.0 is the interface used to hook up the Lipo battery to the Battery socket.

Please find the information is available in the wiki page of Xadow main board.

Thanks and Regards

Unfortunately there is no such information for the Xadow Edison Expansion Board (Xadow Edison Mainboard). But I had already a look at the Xadow standard mainboard v1.0 and assumed the same connector type is used. But there are 11 different connector types at JST homepage with pitch 1.0 mm. What JST series did you use?

Hello,

It is JST 1.0 2 pin SH connector.Its similar to the one sold in the following ebay link.In the JST website it is similar to the one available in the following link

Thanks and Regards

Thank you very much for the valuable information.