Impossible to upload new firmware to rfbee with the uartsbee

Hello,

I try to upload the firmware to the rfbee with uartsbee.

I see the serial in the arduino IDE. I configure the IDE with the board :

Arduino Pro or Pro Mini (3.3v, 8MHz) w/ATmega168

During the upload I received this message :

avrdude: Version 5.11, compiled on Sep 2 2011 at 18:52:52
Copyright © 2000-2005 Brian Dean, bdmicro.com/
Copyright © 2007-2009 Joerg Wunsch

     System wide configuration file is "xadow.app/Contents/Resources/Java/hardware/tools/avr/etc/avrdude.conf"
     User configuration file is "/Users/XXX/.avrduderc"
     User configuration file does not exist or is not a regular file, skipping

     Using Port                    : /dev/tty.usbserial-AJV9OPJ3
     Using Programmer              : arduino
     Overriding Baud Rate          : 19200

avrdude: Send: 0 [30] [20]
avrdude: Send: 0 [30] [20]
avrdude: Send: 0 [30] [20]
avrdude: ser_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding

avrdude done. Thank you.

Can you tell me if it’s normal or not ?

Julien

Could you please show me two pictures about the front and back of RFBee, i need to confirm that what the version of your module.

Jacket

Please find images of my rfbee and uartsbee.

any news ?
IMG_0251.jpg
IMG_0252.jpg

Can someone help me transferring a new firmware ?

Hello,

Can someone is using uartsbee to programming a bee module ? If yes, can you help me solve my issue ?