NFC Shield 2.0 Compatibility

Hi,
I’d like to know if the NFC Shield 2.0 from Seeedstudio is compatible with the Linkit One?
If yes, are there some changes that have to be done, hardware or software?
I tried to connect the two but all I get is “Cannot fint PNXXX board”.

Anyone can help?

Thank you!!

Davide

Please try to use D9 as SPI_SS, thanks~
You need to change the board as well, please refer to
http://www.seeedstudio.com/wiki/NFC_Shield_V2.0#Shield_Interface_Description

Why? What is the problem on using D10, it has the same specifications as D9.

up!

Again, is it possible to use this shield with the linkit one?!

Thank you