Will this work with hardware version 2.52?
Thank you for making this a truly useful device.
To my knowledge, hardware versions went from 2.2 to 2.6. Perhaps you mean
a device that came with app version 2.52? Such a device would have hardware
V2.6, SYS V1.51 and FPGA V2.61. These programs should work fine on that
version or anything later. Keep in mind that the Alterbios plug-in should be installed
on any device with a 2MB drive (prior to hardware V2.72)
See <LINK_TEXT text=“http://www.seeedstudio.com/wiki/DSO_Qua … g_Firmware”>http://www.seeedstudio.com/wiki/DSO_Quad:Upgrading_Firmware</LINK_TEXT> for more info
on hardware/system versions.
Oops, I meant HW 2.72.
Hi Wildcat,
Do I need to save something to avoid a recalibration ?
Sorry, I don’t remember if after an upgrade we have to recalibrate.
Thank you
Calibration routine is the same for these 2 new versions as it was for the previous one (V3.3) so it
will not be affected. V3.4 is the same as V3.3 as far as the entire config file is concerned. V4 adds
some new functions to the menus, these will simply be added to the previous version’s config file when
saved.
If you plan to go back to V3 after loading and saving a config file with V4, the added menu
items could cause menu corruption from arrays being accessed out of bounds if saved in a position
that V3 does not support, so it may be advisable to save a copy of the WPT file in this case before
upgrading.
It’s not a bad idea to save a copy of the config file(s) before upgrading, no matter what versions are
involved, but calibration should not be affected with these latest versions. Also keep in mind if you
have saved any in the additional positions (CONF001.CFG to CONF009.CFG), that although calibration
is not read when loading these files, calibration info is saved in each one, so these could be used as
backups and copied back and renamed to the boot config file (the regular config file “XXXX.WPT”)
if necessary.
Hello everyone,
I bought this little lovely device a few days before. I found it’s really powerful when used with Wildcat4!
I have one question. What is the Wave Calibration of Wildcat4 is doing and how?
I could not find any difference between it is on and off.
My device is HW 2.81 and running with FPGA 281 and SYS B162
Thanks in advance for any help.
Wave calibration (long press left toggle center button with meters off) toggles any amplitude compensation applied
to the waveform so it’s height accurately displays on screen in relation to the grid. Compensation is accomplished by introducing extra “steps” in the waveform. While small and generally not noticeable, under some conditions they can be,
and will detract from what the actual waveform should look like, so they can be turned off if desired. Each V/div range
and channel is calibrated separately, also keep in mind that this won’t do anything unless the entire calibration routine
has been done (Access this by holding down button 2 for more than 3 seconds while the menu is on chA or chB).
This involves using an adjustable voltage source and DMM to calibrate each range. The included user guide explains
how to do this.
Once calibrated, toggling this will simply just adjust the height of the waveform a bit, varying somewhat for each vert
range. With calibration on, a “C” will be displayed in the menu area, off will show “U” (for uncalibrated).
Hi Wildcat,
Thank you for quick reply. Now I can see the difference.
Initially I tried CHANNEL A in 1V/DIV range. Maybe the difference introduced by the calibration is small for that setting. Now I try CHANNEL B in 0.5V/DIV range, and the difference is obvious.
I understand that the stock application always runs in “Wave Calibration ON” setting, and you implemented the ability to turn off that setting into your application.
Thanks again for your kind help, and your continued support for this little lovely device!
Just installed Wildcat’s version 4.0. Nice work Wildcat. Just a couple bugs to report….
- When saving a configuration file (SaveFile 000.CFG), program prompts user with “OK” but immediately increments CH(A) mode setting (DC/AC/DT/TL/RS/) (e.g., DC -> AC, AC -> DT, etc). The saved configuration file must be reloaded, to restore the Channel A mode setting.
- Analog Calibration can be confusing.
- After calibrating DC-offsets and gains, user is incorrectly prompted (at header) to press button 2 to “confirm the re-calibration of Ch_A “. This is confusing, as user might think program needs confirmation of user inputed calibration data. At footer, user is also prompted to use right toggle to “select the next operation”. Header prompt should instead say “restart re-calibration of Ch_A”. If user incorrectly confirms re-calibration, all previously entered data is lost and must be re-entered. User must right toggle twice (<-) to find “Press button 2” or “3” to save calibration data.
- Wildcat User Guide does not cover or explain if Ch_A / Ch_B calibrations should be performed separately or together. Preference is to do Ch_A and Ch_B independently, as the battery level may run low while trying to do both channels at once. Note: Calibration mode is accessed with long-press of button 2, only when Ch_A or Ch_B are selected. If Ch_B is selected, calibration is entered already set for Ch_B, likewise for Ch_A. It is however possible to switch from Ch_A to Ch_B within Calibration mode in order to populate both calibration tables before saving to WPT file.
- Left toggle button beeps can be annoying and should be muted during gain calibration steps. This is especially annoying if no previous calibration data exists.
Device:
Revision(W4.0) by Wilcat
Alterbios 0.4: OK
Hardware Ver V2.70
SYS Ver 1.52
GCCv1.7W4.0 APP(2.51+SmTech1.8+PMOS69 fixes)
Reload parameter from disk
DFU 3.11C.
What’s with the bootup “Reload parameter from disk”. Anyone know what that means?
Yes it does! Never noticed this, if you use the center press left toggle button to save a config file it advances the setting
if any of the menus are set to the 2nd position. I tend to press the same button again (#3) to save config files, and it does not do it that way, so I never noticed it… You don’t need to reload a config file to change it back though, just flip the toggle left. Will be checking into it.
This is a carry-over from the original programming, I never changed it. The original English was a bit strange. I can change the wording around.
I’m not sure if your concern with the battery running low is because it could run out and turn the device off, or if it will affect calibration. As far as calibration is concerned, if I remember right, when saving one channel, the battery level affecting the other channel if it was also calibrated is taken into consideration as far as the battery may now, after time spent calibrating the second channel, be a bit lower. The battery level does not have to be very close to the exhaustion point to set the low level, say maybe 1/4 charge or a bit more should be ok. Battery levels are recorded at calibration
saving point and used as a reference. If the high battery level calibration is done while charging, the VB+ line will be high enough for good interpolation/extrapolation with a low bat level even at 1/2 charge.
OK, I suppose they could be muted as they don’t serve any function. This is again a carry over from the original version, not done on purpose.
This is also a carry-over from the original, it simply means that the start-up config file was found and used to set configuration. If no config file is found it reads “Parameter record not found”. I DID correct the original spelling that stated “Reload parameter form disk”
I appreciate the feedback! Will be posting an update shortly, which will contain a few other fixes as well (in particular a triggering issue while serial decoding in large buffer mode on the 500uS timebase), as well as added SPI and I2C decoding. Will keep all this in mind.
Wildcat,
After reading your comments on the other thread, about ERR with saving CFG files, I noticed that I didn’t have any CFG files on the flash drive. Only had the one WPT file that was created from running the analog calibration. Apparently this was causing the CHA mode fault that you weren’t able to reproduce.
Funny how after saving the CFG and seeing the “OK” prompt, I was able to reload the CFG file settings from the file menu even though there were none; it must have been loading the WPT file instead.
After duplicating the WPT file as 000-009 CFG files, I noticed this fixed the problem. No more CHA mode incrementing when saving a CFG.
Actually, I was able to reproduce the issue, I stated so in my reply. It only does so under some
conditions though: The config has to be saved from the button 3 shortcut, and not from the file menu, the
active (flashing) menu has to be other than the file menu (this gets saved when you use the shortcut
so it goes back to it afterwards) and the final save has to be done with button 5 rather than pressing
button 3 again (button 3 can just be pressed again to save the file). The function that increments the
file save numbers incorrectly increments whatever menu was active when the hold button 3 was pressed,
rather than the file number.
This has already been fixed in the next update.
The #0 config file is the WPT file, the rest of the numbers (1 - 9) are CFG files. The #0 (WPT) file does
not have to have a file already present on the drive to be able to save it, unlike the #1 to 9. This is probably
the file you were saving.
Update: V4.1 (3 slot version only). Added I2C and SPI decoding. User guide has been
updated to explain how to use.
Also fixed a problem with serial decoding under some conditions intermittently triggering in the
500uS time base while in large buffer mode.
Fixed the “advancing menu item” issue while saving config files with left toggle press after selecting
save file function from button 3. Also changed some notifications to improve clarity as was
suggested in a recent post.
NOTE: For SPI decoding, the clock can be either on Ch B or Ch C. Using Ch C as clock allows
decoding both data channels simultaneously on Ch A and Ch B. Prior to hardware V2.72,
these devices had protection diodes that severely limited the bandwidth and timing of the digital
channels. Unless these are removed, at the speeds SPI typically uses, using Ch C the waveform
will be so far out of synch (if it triggers at all), that the function will be useless. For these devices,
Ch B can be used for the clock but decoding will then be restricted to Ch A only.
I2C DECODE: Master sends slave address + request for temp
to temp sensor IC, slave returns 12.0 degrees. NACK from
master ends transfers. Arrow colors show data direction
flow and ACK/NACK
SPI DECODE @ 4Mhz Chart displaying entire buffer
content for both channels can be toggled on/off.
SPI DECODE @ 8Mhz Channel B had to be used for
clock as digital Ch C would not properly display here,
even with protection diodes removed
hi everybody,
I just got this device, HV is 2.81
how do I install this firmware?
I see many files in this .rar other than the .sys, I don’t understand the use of.
Thank you very much for your help,
Roberto
The archive includes the source code and the binaries. For installing wildcats firmware, you only need
one of the hex files. I’ve no idea if you have to consider something when using the new hardware (2.81).
Hi everybody
this is my test with my dso203 - wildcat4.1
Device:
DSO203
Hardware Ver V2.72 8MB
SYS Ver 1.62
APP1 Wildcat V4.1
DFU 3.12C
Usb disk msdos format (with Linux)
Save file bmp cvs buf ecc into 8Mb usb disk in normal mode fft, ecc is ok.
Save file bmp in spectrograph mode not work (err).
Open usb disk (8Mb) in Linux or Windows the bmp image is not valid is impossible open it (view it).
Load the save bmp with the dso is ok, the screenshot is show into the display.
Led for battery charge is only red.
The led remains red even at full charge. Never turns green.
Sorry for my english.
I can confirm a similar problem with hardware 2.70 and Wildcat 4.1, except with slightly different results…
No errors saving and loading BMP files in ‘Spec’ and ‘Map’ modes, however the loaded BMP file’s preview is blank (black) on upper 4/5 screen. Unlike BMP files saved in other modes, these corrupt files cannot be viewed with Windows 7 viewer.
Wondering about the 4-slot version found Wildcat 4.0, missing from 4.1?
Also, was wondering about trigger levels (LEV) for CH© & CH(D). These can’t be adjusted, so shouldn’t the trigger lines be removed and LEV be disabled? Trigger user interface seems confusing for these logic inputs.
Device:
Revision(W4.1) by Wilcat
Hardware Ver V2.70
SYS Ver 1.52
GCCv1.7W4.1 APP(2.51+SmTech1.8+PMOS69 fixes)
Configuration file not found
Have not personally had issues with file corruption (all my devices are HW V2.70
with the Alterbios plug-in with drives formatted on a Windows machine) .
Make sure drives are properly formatted, 2MB drives with 512 byte sectors
(or clusters), 8MB drives with 4096 byte sectors. On a Windows machine, this
should be the default, but if there is a choice it may need to be specified.
BMP’s saved with either the spectrograph or map mode are 64K color types, and
are 4 times the size of BMP’s saved in any of the other modes (16 colors), so
these may get corrupted more easily if there are problems with the drives.
The charging system is completely hardware controlled. The system has access to
the charging state from the charging controller, as well as the battery voltage but
does not control charging. The charge indicator is a red light only, which should go
out when the battery is fully charged. The green light is for standby. My
observations are that the charging system tends to charge these batteries a bit too
much, so I disconnect charging well before the red light goes out.
There is no 4 slot version for V4.1 since compiling this larger version with speed
optimizations would take 5 slots. HW version 2.81 should in theory support this,
with it’s larger documented ROM and remapped FPGA and LOGO code, however
it would over write the FPGA section of earlier devices unless the extra code was
mapped onto undocumented memory. Further issues with this undocumented
“remapping” would be compatibility with HW V2.81 and other programs using
remapped memory.
Trigger level lines for ChC and ChD could be removed, but they are only there when
triggering source is set to that channel, and as such do serve as a trig source indicator.
This is a “carry over” from the original factory programming, never really gave it much
thought.
Thanks,
I just noticed that my previously installed AlterBIOS 0.4 failed to show on the welcome screen. Not sure why this happened. I reinstalled AlterBIOS 0.4 and although it did not reinstall without Windows errors and return RDY, AlterBIOS 0.4 OK now shows on the welcome screen again.
Result: Saved BMP files in Spec and Map modes can now be viewed on both DSO and Windows 7 viewer.
Is there any way to actually uninstall AlterBIOS? Not that anyone would need to do that right now.
Might be interesting if code optimized 4-slot versions were available in different flavors (different program features) since they could be easily swapped via PC link.
If Alterbios was not present, with HW V2.70 and earlier, you will get file
corruption.
The Windows errors, and no RDY is normal, as long as it shows on boot
it should be OK.
Alterbios resides in the system section of the ROM. To remove it, you just
reinstall the Sys file and it will overwrite it.
As far as code optimized 4 slot versions, V4.0 almost completely fills all
4 slots, so adding much of anything spills over to the 5th. V4.0 just lacks
SPI and I2C decode, which take up a good amount of code in ROM. A lot
of functionality would have to be given up to include these to fit in 4 slots.
An alternate solution would be to map the extra code onto undocumented
memory, but this would now have to be hardware specific.
There is a certain amount of ROM above the 4 regular slots that all version
have available in common,this is between the end of the LOGO on earlier
devices and before the FPGA on hardware V2.81, that would ensure
compatibility with all devices, as long as other programs do not also use it.
However not having a V2.81 device to test this with, I wouldn’t be able to
verify the results.