Compiling Wifi library V1.0.42 with Arduino 1.5.8beta gives the following warning
\arduino\arduino-1.5.8beta\hardware\arduino\mtk\libraries\LWiFi\LWiFi.cpp: In constructor ‘LWiFiLoginInfo::LWiFiLoginInfo()’:
\arduino\arduino-1.5.8beta\hardware\arduino\mtk\libraries\LWiFi\LWiFi.cpp:24:18: warning: passing NULL to non-pointer argument 1 of ‘String::String(int, unsigned char)’ [-Wconversion-null]
m_password(NULL)
this comes from the library code
LWiFiLoginInfo::LWiFiLoginInfo():
m_enc(LWIFI_OPEN),
m_password(NULL)
{
}
NOTE: the int LWiFiClass::connect(… ) method has the line
strncpy((char*)context.apInfo.password, loginInfo.m_password.c_str(), VM_WLAN_PROF_PSWD_MAX_LEN);
which would try and apply .c_str() to a NULL object hence the warning appears to be valid
Changing the code to
LWiFiLoginInfo::LWiFiLoginInfo():
m_enc(LWIFI_OPEN),
m_password("")
{
}
removes the warning and the possible null pointer exception
Can this change be incorporated in the next release?