Hello
At this point I just started a project to remotely measure about tanks.
I’ll use an analogue sensor output 0-5V and Linkit ONE board.
I am fairly advanced in Arduino, but only in STAND-ALONE applications or communications XBEE.
I am using the code example to start( reeedstudio l10_web_temp by Waichug Lo), but I do not work properly or not I’m doing wrong.
I have three problems initially:
- the same as:
Compiling Wifi library V1.0.42 with Arduino 1.5.8beta gives the following warning
\arduino\arduino-1.5.8beta\hardware\arduino\mtk\libraries\LWiFi\LWiFi.cpp: In constructor ‘LWiFiLoginInfo::LWiFiLoginInfo()’:
\arduino\arduino-1.5.8beta\hardware\arduino\mtk\libraries\LWiFi\LWiFi.cpp:24:18: warning: passing NULL to non-pointer argument 1 of ‘String::String(int, unsigned char)’ [-Wconversion-null]
m_password(NULL)
this comes from the library code
LWiFiLoginInfo::LWiFiLoginInfo():
m_enc(LWIFI_OPEN),
m_password(NULL)
{
-
The board meets me as you use the address 0.0.0.0
what the browser tells me that is not available -
I want is to constantly check the sensor value, for a similar real-time measurement.
im a new user…somebody can help me?