Hi everybody.
Anybody is experiencing the same issue like me?
Whenever I select the SD card support (SD/SPI switch moved to SD) the board stops to work. It doesn’t execute the sketch, even if the uploading process is successful.
This behavior is the same either if SD card is inserted in the slot or not.
Once the switch is set to SPI the code is properly executed.
Just to be clear, It seems that the code is finally executed, but the LED on PIN13 is always ON when SD is selected on the board. Why you didn’t documented this on the manual? Why the LED on pin 13 is unusable when SD card is selected? I’d appreciate some reply from developers. Thanks