After some stress-testing I found patched 3.64 almost fully functional!
As ricoreyes mentioned, grid intensity can’t be changed, which really doesn’t matter. Also I confirm what santus1983 noticed, buffer can’t be written to SD card. Actually I never managed to write SD with any firmware so it could be a problem with my card. Maybe it doesn’t support SPI or something like that. Anyway directory is created together with .xml file so I believe it’s memory card compatibility issue. There were a lot of this with DSO nano. I’m happy that at least I can write config, it’s useful to setup few profiles as peak hunting, TTL etc.
Thanks for binary patching in the new display driver, it works fine except for the saving of screen dumps etc as described. And the BenF software makes such a difference to the functionality of the scope, further the manual is good (can’t say the original one is very usful).
The process starts alright ie the software is creating the correct file but it breaks when the screen shall be saved to this file. This is not to wonder as the screendump is no longer the one that FredF wrote the export routines for, the display hardware and therefore driver is different. So the SD card routines are most likely OK, what needs to be changed/patched is the screendump stuff reflecting the new driver, then the closing of the file should be successful as well, now the whole thing stops by derailing the processor at the write process.
Just installed this latest fix and it will lock up if I simply move down the list of menus on the right to the bottom and then try and go back up. Anyone else???
rimidalv007 - I too signed up to say thanks for your efforts on the DSO201 software.
I received my nano today and immediately flashed it, all working - thanks again
Same here, I also want to express my thanks to the help of people here - in particular rimidalv007 and of course BenF (hope that he will again show up one day).
And a little question: there is something with a change of install procedure between, I think, the last version of BenF and the latest DSO nano’s. I suppose (hope) that after installing the patched BenF, it is still possible to install other versions in the same way. Likely some of you installed the not-yet-perfect patch and next the improved patch; it works without problems? Just checking, before trying it!
[Edit]: I now installed it (first by mistake the bugged version and then the patched version!) - and it works great!
I am new to all this stuff and have just spent 2 days trying to upgrade the software on my recently purchased DSO201. It has been a nightmare, particularly when one attempt just caused the thing to produce a white screen that gave the impression I had messed the whole thing up permanently. However, I have now sorted the problem and have a much easier to use piece of kit. All thanks to rimidalv007 who is, in my humble opinion, a genius. Thank you. I shall keep an eye on this topic to see if there is more wisdom to come. Thanks again.
My first post, hello to everyone.
I just like to thank rimidalv007 for his expertise and bringing new life to my newly purchase DSO Nano V3.
And of course to all the forum members who contributed their spare time to validate it.
Again thank you all.
New DSO201 owner here (as in, i’m a new owner, not that i own a new nano necessarily!).
Any road, i thought i had everything ready to go on updating to BenF firmware on my Nano but i may have made a boo-boo somewhere (probably by missing a step that i will come to in a bit).
Base on the firmware upgrade screen info, i rightly assumed that i could use hex files directly transferred to the device (one at a time), via USB, to update so I downloaded the V364_APP.hex and V353_LIB.hex and had at it. Or tried to…
On attempting to transfer the first file (V353_LIB i think), the file transferred and, as expected, the device disconnected and…that was all she wrote. The device would not re-connect via USB. I left it for a bit, in case it was ‘thinking’ but nothing changed. I’ve now unplugged it and tried rebooting but i get a ‘digital storage oscilloscope’ title bar and nothing else (at least before i had the purple test trace and it kind of worked in a clunky way).
So, now whenever i plug the device into my laptop and switch on using the ‘-’ key method, the DSO switches to the correct screen and the device (‘DFU…etc’) appears in Windows explorer but immediately vanishes. Therefore i cannot attempt to transfer any other hex files.
Now, i’ve noticed that with Firmware v3.29D, as i have, i should have perhaps used the BENF_P2 file (BenF_3.64APP_3.53LIB_patched_v2.zip) from rimidalv007 but, alas, even though i have downloaded that file i cannot transfer it to the device to the aforementioned ‘vanishing’.
Any thoughts on how i might get my DSO back up and running would be greatly appreciated. Thanks.