rimidalv007, can we have the source code please?
What info contain your boot screen? Try attached files in this post.
Not for now. If I get full newest source BenF fw I will publish my work in one day (after check authenticity)! Reason is: I several times worked on similar things(patching and fixing fwās (on binary level), much complex than this) and publish it and someone get it and continue work on newes versions without publishing. I just want stimulate people to share. If I donāt get BenF new source, I will try to contiune work on this version to improve performance and bug fix depend on my free time. If someone does not have the patience can do it alone. Itās relative easy. I spend about 3-4hours, worked in night between 3:00AM- 7:00AM but job less than 1 hour. At first I had a little familiar with original source.
I had nano just one day and motivate for my work is trigger missing in factory version which is most important for me. I thought to write from zero, but someone alreday did nice job.
LIB301_APP311_2.ZIP (36.3 KB)
It works! You are a genius!
Most excellent work! Now hopefully we can get source for the newest version?
Wow, never imagined Iād see BenF boot up on my nanoā¦
Thank you rimidalv007! Good job!
Single shot works! Now this DSO is usable to me. Unfortunatly, I cannot set/reduce buffer size on low timebase with this version of Benf Firmware?
Was it hard to implement the new display driver? Maybe there could be an easy way to disassemble the hex-file of Benf 3.64 and insert the new display driver too?
[edit]
The first uploaded firmware fell back for me too, but the 2nd posted one worked great.
My browser had some issue, I just forced refresh and found 2-nd version.
rimidalv007, You did it! 3.11 BenF on ILI 9341 LCD! Congratulations! You got my admiration and gratitude!
Now we all hope for the latest and most polished BenF source.
rimidalv007 ā you are amazing! You have great skill. If anyone else can help getting the latest BenF ported to the new display, please ask. Otherwise, we wait for your excellcent work with the latest BenF version.
rimidalv007, great work! But please read the Readme file in BenFās source code. The full license can be found for instance here: gitorious.org/dsonano/dso-firmw ā¦ ce/COPYING
Seems like standard LGPL. Rimidalv007 may publish source but heās not required to do so. Form LGPL wiki:
The LGPL allows developers and companies to use and integrate LGPL software into their own (even proprietary) software without being required (by the terms of a strong copyleft) to release the source code of their own software-parts.
As BenF 3.11 source is available, the modification to the display driver doesnāt have to be.
He is required by law to distribute the modified source code, everything that is derived from the BenF source code.
āintegrateā means here using together, but with a clear distinction between the LGPL-licensed code and the other code that is used in the system. It does not allow freely mixing the LGPL code with other code and distributing the result without source code.
What the LGPL allows is using the unmodified code as a library (or software module) in an otherwise proprietary (or other non-LGPL) software system. For example you can write an APP from scratch and use the BenF LIB as-is. But any modification you make to the LIB to accommodate this would be covered by the license and you will need to provide the modified LIB source code.
How about patching binary files?
I was thinking ā¦
And if we make one fund with donations to make the software more usefull, to pay who are working on it ???
Those peoples that make contributions will have the rights to use the new firmware.
Or something like thisā¦ I think that who is working on it need make some money, is like a regular jobā¦
I see that many of us can pay to have one more usefull device, this little DSO is an amazing equipment that need a better firmware. I really donāt understand why Seedstudio donāt make a better firmware !
Paulo
It is still derivative work, and is covered if the binary files were distributed under the LGPL. Anyway, in this case the source code was also consulted.
I believe BenF gave us his software under this license because he did not want someone to distribute modified versions without sharing the code. Since it is his code, he owns the copyright to it and decides how we can distribute it and any modified versions of it. I donāt think violating his rights will encourage him to share more of his codeā¦
Instead of pestering for the source on the modified BenF 3.11, letās persuade BenF to let rimidalv007 patch 3.64!
He did say that heād release the patch for that version for further development, isnāt that the goal?
paulo3,
I believe normal donation options would be sufficient. For instance, ātestdiskā saved me a lot of time. I was so happy with it that donated the same day. Author made effort to make donation system fast and easy.
tormod,
I understand that thereās a difference between usage of LGPL based software and making project based on it. When it becomes derivative project, itās covered with section 2 of the license rather than section 6.
The situation is weird and you know it. BenF closed his source after 3.11. Of course he can do this as an author. Now we got situation when rimidalv007 contributed his time and knowledge to integrate new procedures into LGPL licensed software. As ricoreyes said, it would be great if BenF open-sourced 3.64. Wellā¦ Actually if BenF would like to use patch, his firmware would have to become open-source again. Right?
3.64 is closed-source. I donāt know what if binary file got patched. It doesnāt include any source to it. I donāt even know if it was licensed. Was it?
But hey, what do I know, letās drop this
Good news! LIB3.53-APP 3.64 is cured
It will be available in coming days. Due to complaints about licensing I will wait for some time to BenF or someone else possibly answer about their plans. Anyway, you will have the latest version on your newest nano toys. In the meantime, Iāll test cured fw and fix possibly bugs because I worked a lot on binary files. For now, all looks good.
BenF v3.64 in action:
[url=http://img145.imagevenue.com/img.php?image=311139346_MyNano_122_350lo.JPG][img=http://img145.imagevenue.com/loc350/th_311139346_MyNano_122_350lo.JPG][/url]
Thanks a lot, rimidalv007 !!!
Please tell how we can make donations to you by your work, finally soon I can use my New DSO like my old model ! Iām sure that others will contribute too !
My congratulations !
Paulo
+1
In a dayās work youāve done what weāve all been scratching our heads over for months. If you setup a payment account Iād gladly donate.
You patched binary file. Now thatās some serious skill
Seriously, congratulations.
Iāll gladly donate for both, firmware and patch, if I get a chance.
As for licensing, I donāt believe BenF would speak here, he havenāt respond to anyone for some time now.
But I can paste first two paragraphs He wrote in the instruction manual to his firmware, that would clear situation a bit:
Link: benfwaves.googlecode.com/files/ ā¦ 0Guide.pdf
From wiki: