[size=150]Introduction[/size]
ArduinoPhone is a simple wireless phone, which has the simple functions of wireless phone, such as calling, receiving a call, sending and receiving texts and time display.
Communication function can be achieved through GPRS Shield, and display function through TFT Touch Shield. A complex firmware is applied to realize UI management, with the functions of click and swipe.
The difficulties are:
[size=150]Hardware[/size]
1 Modules
Arduino/Seeeduino
GPRS Shield
TFT Touch Shield
Grove – RTC
Self-madec7.4V Lithium battery charging board ( circuit diagram will be shown), can also use 9V battery as power supply.
2 Hardware Connection
GPRS Shield communicates through hardware serial. TFT Touch Shield is V1.0 (non-SPI interface). With simple code modification, it’s compatible with TFT Touch Shield V2.0. Grove – RTC use I2C interface.
Is there enough memory left in the Arduino Uno to support adding audio and basic voice call functionality? I am interested in this to build an Arduino cell phone. is it doable? if so, which Grove parts would you recommend to add voice functionality to it.
Hey little boy, do you want to counteract my efforts, i must give you color see see
by the way, the man upstairs is author of Arduino Phone, and he is a Fatty.