Raindrops - a little toy, which is based on the interplay of Arduino, Rainbowduino and an accerlerometer. As pictures can tell you more than hundreds of words maybe you should just start by watching my little video:
Hi, your game looks great. Iād like to test out your code, but the client.pde wonāt compile without the āRainbowduino.hā library. Can you post that as well on your github page please? Thanks.
Actually, Iāve got another error asking about the Accelerometer.h library. I found another one online, built by Atmel for AVR32. I guess itās not the right library because the code still doesnāt compile. I looked a bit on the Arduino.cc page but no luck there. Would you mind pointing me in the right direction or posting that library as well? Thanks again.
sorry I forgott to mention, I used the accelerometer Lib on seedstudions website, see here: seeedstudio.com/depot/wiimot ā¦ p-107.html
copy this into your source or library folder as well, now it should work!?
Thanks. I actually just hacked out all the accelerometer code to try to get it to even run. It certainly did, and looked great.
But, the display looked kind of dim. Any ideas why? Iāve loaded up different firmware and the original Seeedstudio rainbow.h library as well as the one youāve used (rainbowduino.h I think). Of all, it looks like the seeed example on using the Rainbowduino to control their 12V light strips gives the highest brightness output. http://www.seeedstudio.com/blog/?p=512 The problem with this example is that I canāt figure out how to make use of all the LEDs in the matrix, itās just controlling 2 rows of them.
Any thoughts on why the LEDs are so much dimmer when Iām running your code?
BTW, I really like how youāve coded the game. Itās pretty brilliant way of tracking collisions and running the game from what I can tell. Nice work!
I changed 31 to 32 the matrix is shiny bright by colors change. really wired, donāt know whatās wrong have to dig deeper into it, unfortunately Iām quite busy right now, but itās on my TODO list to check it outā¦ Iāll let you knowā¦
Raindrops
This is the Raindrops Rainbowduino Game. Itās a Rainbowduino connected via I2C to an Arduino with an Accelerometer. The current position/movement is determined and send via the I2C Bus to the Rainbowduino. With that you can move the red dot on the Matrix and avoid hitting the falling blue raindrops. But if you do so, the game is over. Tilting the devices influences the speed of the drops as wellā¦ Have fun!
Used Components:
Rainbowduino
8x8 RGB LED Matrix
Accelerometer ADXL330
Arduino
Usage:
First, get the Rainbowduino.h Library and put it into your Arduino IDE Library (or in the same folder as the sources). Second, do the same with the Accelerometer Library found here.
Now, compile both sketches and upload the Server.pde sketch to the Accelerometer, upload Client.pde to the Rainbowduino. You are ready to go! Have fun!