Maple Mini and Grove

Hello,
Is anyone here who use Maple Mini boards as a control units for Grove bricks?

I just started with Maple Mini and SerialLCD and its work.
Planed: Compass, Stepper motors, etc.

It will be great to exchange experiences with others and build libraries for other bricks.

First - is Grove_SLCD library. This is ported from library for Arduino.
Tested with Maple Mini - on serial ports 1,2 and 3.
When you connect SerialLCD module to Maple Mini - please remember that you need external +5V power supply for SerialLCD module - on Maple mini you have only +3.3V.

Sample .pde:

/*
 Grove_SLCD Library - Hello Grove
 
 Demonstrates the use a 16x2 LCD SerialLCD driver from Seeedstudio.
 
 This sketch prints "Hello, Grove!" to the LCD and shows the time since reset.
 
 Library originally added 16 Dec. 2010 by Jimbo.we  http://www.seeedstudio.com
 */

// include the library code:
#include <Grove_SLCD.h>

SLCD SLCD(2); // here - serial port number is selected

void setup() {
  // set up
  SLCD.begin();
  // Print a message to the LCD.
  SLCD.print("Hello, Grove!");
}

void loop() {
  // set the cursor to column 0, line 1
  // (note: line 1 is the second row, since counting begins with 0):
  SLCD.setCursor(0, 1);
  // print the number of seconds since reset:
  SLCD.print(millis()/1000,DEC);
}

Best,

Marek
Groove_SLCD.rar (2.84 KB)

Dear customer,

Thanks for your sharing.
After your project, suggest you can go to instructables.com to attach that.
And we would put example to our Recipe.

Best regards,

Yuri