Dielectric Constant of PCBs

Moderators: violet, carmen.zheng

Post Reply
simon.newtonlabs
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Mon Mar 09, 2015 8:06 am

Dielectric Constant of PCBs

Post by simon.newtonlabs » Mon Mar 09, 2015 9:20 am

I am working on an impedance critical PCB, and I was wondering what the dielectric constant for the 0.6mm PCB is. Thanks, and have a great day, Simon.

catherine12297
Pre-kindergarten
Pre-kindergarten
Posts: 17
Joined: Wed Nov 28, 2018 7:37 pm

Re: Dielectric Constant of PCBs

Post by catherine12297 » Thu Dec 06, 2018 6:35 pm

You can look up the specs of the material at the PCB producer. The dielectric constant doesn't depend on the frequency but the loss in the material does. If the application has to be very precise go for Rogers material otherwise FR4 is good until several GHz (assume er=4.5). When working with microstrips also consider the tolerances of the trace widths. If you get close to the minimum trace width the manufacturing tolerances will screw things up.

Post Reply