MRAA support for user button A6

Hi,



is there any way to access User Button A6 via MRAA?

Wiki references two different ways of accessing GPIOs - MRAA for the header GPIO 8Pin Header and input device /dev/input/event0



Is there an access functionality which gives me isr functionality for A6 (not to access read_loop() over and over)



Thx and best regards

Hi there,



Sorry, the current system does not support to use mraa to read the on board button status. I will give feedback to software engineer and see if it is possible to add the function into next release. thanks.



Bill