Mic Array v2.0 recording high pitch noise

I have used the Mic Array v2.0 for a while now. One thing I’ve noticed is that the first channel, i.e. the beamformed channel for ASR, always contains some hight pitch noise. See the attached picture of the spectrogram.



I have tried tuning the parameters but couldn’t get rid of it. Seems it has picked up some interferences.



For the reference, I am using Raspberry Pi 3 for recording. AGC and Noise Suppression are both turned on. Below is a link to the audio file



<LINK_TEXT text=“https://www.dropbox.com/s/zn66l91bich6o … g.wav?dl=1”>https://www.dropbox.com/s/zn66l91bich6oms/mic-array-recording.wav?dl=1</LINK_TEXT>



Any assistance is appreciated.



Best

Ning
mic-array-recording.png

Hi,



Further to my problem I’ve done some investigation and believe the high pitch noise comes from the USB. As you can see from the spectrogram the noise has a perfect fundamental frequency at 1kHz and harmonics at multiples of 1kHz. I read some articles with the following explanation:

Any suggestions?



Best

Ning