need the schematics of the respeaker core v2
Moderators: lily.li, violet, seth.welday
need the schematics of the respeaker core v2
can you provide the schematics of respeaker core v2 so that i can get a clear understand of how to configure the interface as my need?
Re: need the schematics of the respeaker core v2
Hi there,
We do not open source respeaker core v2 this moment. if you have any specific interface related questions, we can check it for you. thanks for understanding.
Bill
We do not open source respeaker core v2 this moment. if you have any specific interface related questions, we can check it for you. thanks for understanding.
Bill
Re: need the schematics of the respeaker core v2
OK. I think it was CDC device though the only OTG device found is configured as a hub like the pasting below.
Is this the right port of the USB OTG interface?
T: Bus=01 Lev=00 Prnt=00 Port=00 Cnt=00 Dev#= 1 Spd=480 MxCh= 1
B: Alloc= 0/800 us ( 0%), #Int= 0, #Iso= 0
D: Ver= 2.00 Cls=09(hub ) Sub=00 Prot=01 MxPS=64 #Cfgs= 1
P: Vendor=1d6b ProdID=0002 Rev= 4.04
S: Manufacturer=Linux 4.4.138-respeaker-r0 dwc2_hsotg
S: Product=DWC OTG Controller
S: SerialNumber=30040000.usb
C:* #Ifs= 1 Cfg#= 1 Atr=e0 MxPwr= 0mA
I:* If#= 0 Alt= 0 #EPs= 1 Cls=09(hub ) Sub=00 Prot=00 Driver=hub
E: Ad=81(I) Atr=03(Int.) MxPS= 4 Ivl=256ms
Re: need the schematics of the respeaker core v2
Hi there,
Here is the schematic for the usb/pwr. thanks.

Bill
Here is the schematic for the usb/pwr. thanks.

Bill