RPI 4 mic array with extension cable

I bought a RPI 4 mic array (hat) and would like to use it not directly plugged into the RPI. I would rather use it 10-15 cm away from the RPi itself and connect it via a cable (40 pin IDE Cable) or direct wiring of the needed contacts… Now here’s my problem:

If I connect it through a cable, the PI doesn’t recognize the device.

If I plug it directly into the GPIO header, it works fine.

Is there no way to connect the hat with a cable instead of plugging it in directly?

Or were just all my cables faulty?!

Ok. Sry for the post, seems to have been a wiring problem on my side :wink:

Hmm. I’ve got a third (not at once) cable connected. It’s approximately 20cm long. And now I can dress the LEDs but can’t seem to connect the mics…

Is cable length significant for the mic operation?