ReSpeaker Core V2 Mic Processed Audio Output

Hi I am looking to get audio out of the core v2 3.5mm ,like you can with the mic array. I also need to be able to feed analog audio into the device to add it to the AEC reference. i am planning on using this in a car, and i would like to have the device ignore any audio from the radio while i am speaking. I have my device setup and i can VNC and putty ( Serial ) into it as well

Support, can you help? I purchased the Core v2 with the plan to use it as a mic array and voice assistant with everything running on the device locally.

Hi there~,



The ReSpeaker Core v2.0 does not support this functions. I would suggest you buy the respeaker mic array v2.0 and raspberry pi. It can support your application. thanks.

There is no way to send processed audio out the 3.5mm using software?

Hi there~



For ReSpeaker core v2.0, we do not have the solution to send out through 3.5mm audio port.

For ReSpeaker Mic array v2.0, you can follow Q5 of the FAQ to update the firmware and you can get the audio output from 3.5mm audio port. thanks.

<LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_M … _v2.0/#faq”>http://wiki.seeedstudio.com/ReSpeaker_Mic_Array_v2.0/#faq</LINK_TEXT>