ReSpeaker 4 Mic Array firmware

info about ReSpeaker series products

Moderators: lily.li, violet, seth.welday

Post Reply
Anonymous
Kindergarten
Kindergarten
Posts: 92
Joined: Mon Jun 03, 2019 10:58 am

ReSpeaker 4 Mic Array firmware

Post by Anonymous » Wed Mar 20, 2019 10:54 pm

Hi,
we are using the respeaker v2.0 4 mic array for an audio tracking project and were wondering if there is a way to disable the voice processing entirely so as not to filter out other noise. Do any of the firmware binaries work well for this, or are there other parameters that can be set to ‘off’ to accomplish this?

Seeed Tech Support
Pre-kindergarten
Pre-kindergarten
Posts: 0
Joined: Mon Jun 03, 2019 10:51 am

Post by Seeed Tech Support » Thu Mar 21, 2019 9:29 am

Hi 

Yes, you can use the 6 channels firmware and select the channel 1~4, they are the raw audio from 4 mics. there are some 6 channels firmware and you can select the best one fits your project. 
http://wiki.seeedstudio.com/ReSpeaker_M ... e-firmware 


firmware
channels
note



1_channel_firmware.bin
1
processed audio for ASR


6_channels_firmware.bin
6
channel 0: processed audio for ASR, channel 1-4: 4 microphones' raw data, channel 5: playback


6_channels_firmware_6.02dB.bin
6
same as 6_channels_firmware.bin, but 4 microphones have a 6.02dB gain


6_channels_firmware_12.04dB.bin
6
same as 6_channels_firmware.bin, but 4 microphones have a 12.04dB gain


48k_1_channels_firmware.bin
1
48k sample rate, 1 input channel


48k_6_channels_firmware_6.02dB.bin
6
s48k sample rate, 1 input channel, 6.02dB gain



Thanksbest rgdsBill

Post Reply