Respeaker Core v2 as Bluetooth Device

Hello,



i have searched nearly the whole web and tried many tutorials but i just couldn’t find a setup that i can use my Respeaker Core V2 as a Bluetooth Device so i can play music from my phone to my respeaker.

I have attached a speaker to the 3.5mm Audio Jack and i just want to play audio like a very basic bluetooth speaker.



I was wondering if there is a solution for that, because i can image that this is something that more people would wish for or even need.

Are there any attempts to solve this.

I am ready to help or finish development on such a solution, but of course i would need some one who points me to the right direction.



Thanks in advance and hopefully we can build a good solution.



Peter

i have the same problem as you i want to use my respeaker core v2 as a bluetooth device to connected to wifi through a phone application . i searched a lot but could not find anything related but i do recommand searching for solution for raspberry pi and then accomandate the result to respeaker core v2.

if you have any result please keep me posted.

Hi,

i just setup a new Respeaker Core V2 with a clean image and it figured out that the installed service already works!

See the attachment!

So all you have to do is follow this setup guide: <LINK_TEXT text=“http://wiki.seeedstudio.com/ReSpeaker_C … reparation”>http://wiki.seeedstudio.com/ReSpeaker_Core_v2.0/#preparation</LINK_TEXT>



Best regards,

Peter