Question About the Oscillator in ReSpeaker 4-Mic Array

Hi Seed Tech Support Team,



Currently, I am doing a project using the ReSpeaker 4-Mic Array. I found that this board has its own oscillator. When connected to the Raspberry Pi, it will use its own oscillator while recording. In my project, a speaker is connected to the Raspberry Pi and the 4 microphones record ultrasonic signals transmitted by the speaker. When analyzing the recorded signal, I found that the sampling rate of the transmitter and receivers are not exactly the same, and I think it is because the two boards are using two separate oscillators. So can I program to the Raspberry Pi so that the ReSpeaker 4-mic Array and Raspberry Pi can use the same oscillator (any of the 2 oscillators)? Or is there any other way to do that?



Thanks a lot!

Hi there,



the speaker will filter some high frequency signals(48Khz). But it only passes the frequency below 16khz. then you record the 16khz signals. you can consider to buy grove-ultrasonic sensor to do the experiment. thanks.

http://wiki.seeedstudio.com/Grove-Ultrasonic_Ranger/