The problem of wifi connect with ap

info about ReSpeaker series products

Moderators: lily.li, violet, seth.welday

Post Reply
nj1865
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat Feb 02, 2019 2:17 pm

The problem of wifi connect with ap

Post by nj1865 » Sat Feb 02, 2019 2:19 pm

我们公司设置了2.4G和5G混合的无线ap,没有密码。笔记本和手机都能正常搜索到,信号满格,连接也正常。
但是ReSpeaker Core V2.0搜索的话,经常搜不到信号,就算搜到,信号也不太好。而且一直连接不上。
有时候在连接过程中,信号也会丢失。
而公司的另外的树莓派和firefly的开发板均能正常连接此AP。

The follow text is translated by baidu.

Our company has a wireless AP with both 2.4G and 5G, which with no password.
It's signal is full on my notebook computer and mobile phones,
And it can be searched and connected by notebook computer and mobile phones quickly.

But when I use ReSpeaker Core V2.0 to search it, the signals are often not found. Even if it is found, the signals are not very good. And it's never connected.
Sometimes the signal will be lost during the connection. We have two boards, Both of them like so.

But the raspberry pi and Firefly development boards are able to connect to this AP.
What can I do for this?

Post Reply