WHAT IS 3D PRINTING? HERE’S WHAT YOU NEED TO KNOW.

new product release, exhibitions/ trade shows, promotions, contests, or any other contents (videos/tutorials) that are useful to the community.

Moderators: lily.li, violet

Post Reply
User avatar
anson.he
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Sat Sep 29, 2018 10:45 am
Are you a staff member of seeedstudio?: yes
Which products/projects are your favorite?: Arduino, ESP8266, IoT Solutions and general cool stuff :)

WHAT IS 3D PRINTING? HERE’S WHAT YOU NEED TO KNOW.

Post by anson.he » Fri Apr 26, 2019 11:44 am

Have you ever wondered how 3D printing works, or just what 3D printing can be produced nowadays? You’ve come to the right place: we’re going to cover some basics of how do 3D printing work, what can you do you with 3D printing, and how this could accelerate your projects.

What is 3D Printing? Source: CNN, Youtube

3D printing, also known as additive manufacturing is an innovative manufacturing technology that allows you to build/create a physical three-dimensional object from a digital model. A 3D printer is simply a machine that can take a digital 3D model and build such three-dimensional object by depositing material layer by layer in accordance to the digital file.

Digital Files
In order to print something, first you’ll need a digital 3D model of the object that you want to create, which you can design in 3D modeling programs (CAD – Computer Aided Design), or even with the use of a 3D scanner to scan the object you would like to print. Many programs can create these files, including Solidworks, Blender, Tinkercad and etc. which all have their own strengths and useful for different purposes. The digital file instructs the printer exactly how to create the 3D object. It does this by dividing the object into layers and describing the dimensions of each layer with great accuracy.

Image

How does it work?
Once we have the digital file ready, we can simply load it to our 3D printers, but how does the printer work? Usually, desktop 3D printers have to accurately replicate each layers described in the file. That means that it needs enough free and clean space to construct the object, which is why most desktop 3D printers are in a box, or compartment to work in. While technologies vary, these machines usually employ nozzles, or laser to lay down the material and then set or cure it for each layer. As you can imagine, these printers must be calibrated very carefully.

Image
FDM 3D Printing on the go

Types of 3D Printing
3D printing technologies have been around for decades. An important turning point was at 2009, when a consumer-friendly type of 3D printing called FDM (Fuse Deposition Modeling) became publicly after that patent expired. That led to a boom in affordable 3D printing devices, and even today the most common used version of 3D printing is still FDM. However, there are many different types of 3D printing used in various fields.

Fuse Deposition Modeling(FDM)

FDM uses a simple nozzle to extract plastic filament which cools down into the 3D printed shape. This is the cheapest version of 3D printing, where it is the technology that majority of the desktop 3D printers are using. Since it only needs a box, a nozzle, and a system to turn the digital 3D model data into movement, this type of printer can come in many different sizes.

For this, we’ve launched a series of affordable FDM desktop 3D printers on our Seeed’s Bazaar site ranging from 150*150*150mm all the way up to the industrial sizes allowing you to create what you want/need. If you would like to buy you own desktop 3D printers, here’s where to look at.https://www.seeedstudio.com/manufacturi ... nting.html

Image
Some 3D printed prototypes/components presented at x.factory Dongguan!

Stereolithography (SLA)

Technically the first type of 3D printing to be invented back in the 1980s. SLA beams a laser at a reactive liquid resin so it instantly hardens. The object is then pulled out of a vat of this liquid, layer by layer. SLA is capable of much greater detail than FDM, but the printing process is also more complex and much more expensive.

What can you do with 3D printing
It’s hard to find a field that 3D springing that hasn’t been affected by 3D printing. Manufacturing processes around the world have adopted 3D printing techniques to help solve their problems and increase efficiency. When used in mass production, 3D printing tends to be cheaper than any other method. When used to create prototypes, it’s typically the fastest option.

Custom Models: Create customised products that are completely tailored to your needs in terms of size and shape. Companies like 3D shoes manufacture 3D printed shoes on demand, with plenty of customisation options.

Rapid Prototyping: 3D printing makes it possible to quickly create a model or prototype to help engineers, designers and companies to visualise and get iterative feedback on their design at a short period of time.

Lower Cost: The cost of 3D printing end use parts and prototypes is low thanks to the materials and technology used. Production time and material waste are reduced too since you can print models multiple times using only the material needed.

Image

But for now, let see what you can create with these machines available and start exploring the joy of digital fabrication! https://www.seeedstudio.com/manufacturi ... nting.html

User avatar
salmanfarisvp
Pre-kindergarten
Pre-kindergarten
Posts: 22
Joined: Sun May 20, 2018 2:02 am
Are you a staff member of seeedstudio?: no
Which products/projects are your favorite?: Linklt One , BeagleBone Green , ReSpaker
Contact:

Re: WHAT IS 3D PRINTING? HERE’S WHAT YOU NEED TO KNOW.

Post by salmanfarisvp » Wed May 29, 2019 2:14 am

Nice explanation and thanks for sharing Anson.he :)

Post Reply