Streaming audio through the Bluetooth bee

new product release, exhibitions/ trade shows, promotions, contests, or any other contents (videos/tutorials) that are useful to the community.

Moderators: lily.li, violet

Post Reply
worldsoldier5
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Fri Mar 29, 2013 11:37 am

Streaming audio through the Bluetooth bee

Post by worldsoldier5 » Fri Mar 29, 2013 11:40 am

Dear,

I am trying to have my laptop connected to a speaker through Bluetooth. I have the SeeedStudio Bluetooth Shield ( http://www.seeedstudio.com/wiki/index.p ... oth_Shield ) that is mounted to the Arduino Uno which then output music to the Speaker. I am not worry about the output right now, I am having problem streaming the music from my computer. My computer detects the Bluetooth shield but I am not sure how to stream audio from it. I tried to use putty but with no luck. Does anyone have a clue how to solve my problem? Is it possible to use A2DP with the Bluetooth bee?
Thank you
Mat

strigoi8183
Pre-kindergarten
Pre-kindergarten
Posts: 11
Joined: Mon Apr 22, 2013 12:52 pm

Re: Streaming audio through the Bluetooth bee

Post by strigoi8183 » Thu Apr 25, 2013 8:01 am

The datasheet for the bluetooth module that is onboard the bluetooth shield has some information pertaining to exactly what you have described above....

2.Feature
Radio Transceiver
Typical –80dBm sensitivity
Up to +4dBm RF transmit power with power level control
Fully Qualified Bluetooth V2.0+EDR(Enhanced Data Rate) 2Mbps Modulation
Integrated 15-bit Linear 8KHz Sample Frequency Audio CODEC in one chip
Internal 6Mbit ROM
Low Power 1.8V Operation
Integrated Switch-Mode Regulator (DC To DC)
Integrated Battery Charger With Programmable Current
PIO control
Standard HCI(UART or USB)
4.2V Tolerant LED Drivers With Intensity Control
UART interface with programmable baud rate
Basic module without antenna
Basic module as SMD type
With Audio Out & Audio in
Package option
Edge connector

3. Summary of Benefit
Complete Bluetooth Solution
Complete 2.4GHz radio transceiver and baseband
CSR Bluecore 04-Audio ROM, single chip bluetooth system with CMOS technology
Adaptive frequency hopping feature (AFH)
Smallest footprint, 27mmX13mm
Simplify overall design/development cycle
Full speed Class 2 bluetooth operation
Class I support using external power amplifier
Low power standby modes to enable high efficient power management
High performance radio transceiverz Low overall system cost
Application
Mouse
Automotive Hands-Free Kits
Cordless headsets
Software
Support CSR bluetooth stack
Design for Client

You can view more at the following link
http://www.seeedstudio.com/wiki/images/ ... module.pdf

rootsys6
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Feb 18, 2015 8:37 pm

Re: Streaming audio through the Bluetooth bee

Post by rootsys6 » Wed Feb 18, 2015 8:41 pm

The Arduino Phone Design and Development Innovation Competition,is now officially launched.    
We welcome Arduino enthusiasts, makers and artists from all sectors of society to take part in this activity. This activity is aimed at carrying out personalized version of Arduino Phone V2.0 design and encouraging the users to take notice of maker’s spirit and participation spirit.
ahsan

alina06
Pre-kindergarten
Pre-kindergarten
Posts: 6
Joined: Thu Apr 11, 2019 3:34 am

Re: Streaming audio through the Bluetooth bee

Post by alina06 » Thu Apr 11, 2019 3:39 am

We welcome Arduino enthusiasts, makers and artists from all sectors of society to take part in this activity. This activity is aimed at carrying out personalized version of Arduino Phone V2.0 design and encouraging the users to take notice of maker’s spirit and participation spirit.

Post Reply