Hi,
I recently got the WIO Tracker and ran several of the examples and they worked. To test sensor data collection I want to run the 6 axis accelerometer & gyroscope sensor <LINK_TEXT text=“http://wiki.seeedstudio.com/Grove-6-Axi … ch-support”>http://wiki.seeedstudio.com/Grove-6-Axis_AccelerometerAndGyroscope/#tech-support</LINK_TEXT> (it is the one I have) on the WIO Tracker. The example that comes with the WIO Tracker library is for the 3 axis accelerometer.
I would like to see an example showing how to read the I2C data from the 6 axis sensor I have.
I tried customising 6 axis sensor code to work on the WIO tracker, but I get no output. Here it is below. Would you let me know what I am doing wrong.
Thanks!
[code]
/*****************************************************************************/
// FreeFallDetect.ino
// Hardware: Grove - 6-Axis Accelerometer&Gyroscope
// Arduino IDE: Arduino-1.65
// Author: Lambor
// Date: Nov,2015
// Version: v1.0
//
// Modified by:
// Data:
// Description:
//
// by www.seeedstudio.com
//
// This library is free software; you can redistribute it and/or
// modify it under the terms of the GNU Lesser General Public
// License as published by the Free Software Foundation; either
// version 2.1 of the License, or (at your option) any later version.
//
// This library is distributed in the hope that it will be useful,
// but WITHOUT ANY WARRANTY; without even the implied warranty of
// MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the GNU
// Lesser General Public License for more details.
//
// You should have received a copy of the GNU Lesser General Public
// License along with this library; if not, write to the Free Software
// Foundation, Inc., 51 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA
//
/*******************************************************************************/
#include “SparkFunLSM6DS3.h”
#include <Wire.h>
#define CLEAR_STEP true
#define NOT_CLEAR_STEP false
#define GrovePowerPin 12
//Create a instance of class LSM6DS3
LSM6DS3 lsm6ds3( I2C_MODE, 0x6A ); //I2C device address 0x6A
uint16_t detectCount = 0;
void setup() {
SerialUSB.begin(9600);
pinMode(GrovePowerPin, OUTPUT);
// write high to grove power pin to enable all the Grove ports,
// or only Grove D2 port is usable.
digitalWrite(GrovePowerPin, HIGH);
if( lsm6ds3.begin() != 0 ){
SerialUSB.println(“Device error”);
}
else{
SerialUSB.println(“Device OK!”);
}
if(0 != config_free_fall_detect())
SerialUSB.println(“Fail to configure!”);
else
SerialUSB.println(“Success to Configure!”);
}
void loop()
{
uint8_t readDataByte = 0;
//Read the wake-up source register
lsm6ds3.readRegister(&readDataByte, LSM6DS3_ACC_GYRO_WAKE_UP_SRC);
//Mask off the FF_IA bit for free-fall detection
readDataByte &= 0x20;
if( readDataByte )
{
detectCount ++;
SerialUSB.print("Free fall detected! ");
SerialUSB.println(detectCount);
}
delay(10);
}
int config_free_fall_detect(void)
{
uint8_t error = 0;
uint8_t dataToWrite = 0;
dataToWrite |= LSM6DS3_ACC_GYRO_BW_XL_200Hz;
dataToWrite |= LSM6DS3_ACC_GYRO_FS_XL_2g;
dataToWrite |= LSM6DS3_ACC_GYRO_ODR_XL_416Hz;
error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_CTRL1_XL, dataToWrite);
error += lsm6ds3.writeRegister( LSM6DS3_ACC_GYRO_WAKE_UP_DUR, 0x00 );
error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_FREE_FALL, 0x33);
error += lsm6ds3.writeRegister( LSM6DS3_ACC_GYRO_MD1_CFG, 0x10 );
error += lsm6ds3.writeRegister( LSM6DS3_ACC_GYRO_MD2_CFG, 0x10 );
error += lsm6ds3.writeRegister(LSM6DS3_ACC_GYRO_TAP_CFG1, 0x01);
return error;
}
[/code]