Hi Guy,
Im from Germany and need some help. Im bought a “Wio GPS Board” to built up a tracking Solution. Now I figured that not all Arduino Library are being supported by seeed especially not TiniGSM is not supported with the onboard MC20 Modem.
I need the board to built up a simple tracking solution with GSPs and Temperatur which should be sent to ThingsBoard Cloud.
This Cloud support JSON API for the telemetry upload like this with a “Access_TOKEN-ID” to publish telemetry data.
The stated that the format should look like this.
http(s)://host:port/api/v1/$ACCESS_TOKEN/telemetry
{“key1”:“value1”, “key2”:“value2”}
Has someone an idea or reference coding how this can be realized with the Wio to sent HTTP Posting?
Markus
Hi,
Which development board are you using? Wio Tracker or something else?
I use the following board:
<LINK_TEXT text=“https://www.exp-tech.de/module/wireless … -YQAvD_BwE”>https://www.exp-tech.de/module/wireless/bluetooth/8232/seeed-studio-wio-tracker-gps-bt3.0-gsm-arduino-compatible?gclid=CjwKCAiApOvwBRBUEiwAcZGdGIZOYEYSh08rdtzKz9ul0vEEY0j0AtSQuqMbxX2Md3zHz0klG-bAUxoCX-YQAvD_BwE</LINK_TEXT>