Unable to update firmware on Wio Node

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
alan.2.tucker
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Apr 25, 2019 6:14 pm

Unable to update firmware on Wio Node

Post by alan.2.tucker » Tue Apr 30, 2019 6:05 pm

I have multiple Wio Links set up sometime ago no problem.

Now trying to add a new Wio Node with a Grove Magnetic Switch connected to UART0/I2C0/D0

When trying to update the firmware either through the iOS app or via the API I get the same error displayed:

Code: Select all

sh: 1: make: not found
Even fails if I use one of the Grove modules previously configured correctly (PIR)

bill.yu
Junior-7
Junior-7
Posts: 707
Joined: Mon Apr 02, 2018 11:05 am

Re: Unable to update firmware on Wio Node

Post by bill.yu » Wed May 08, 2019 2:29 pm

Hi there,

I just tested it and it works now with global server, do you still have the issue? thanks.

Post Reply