help

Simplify IoT Development.

Moderators: lily.li, violet, seth.welday

Post Reply
ousmanedeme7313
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Sun Jan 13, 2019 11:12 pm

help

Post by ousmanedeme7313 » Thu Aug 22, 2019 2:46 am

hello, I have a probleme when i upload my skech

Arduino: 1.8.4 (Windows 10), Card: "Wio GPS Board"

CAUTION: The category '' in the FlashStorage library is invalid. Definition on: 'Uncategorized'
The sketch uses 20104 bytes (7%) of program storage space. The maximum is 262144 bytes.
An error occurred while uploading the sketch

This report could be more detailed with
the option "Show detailed results of the compilation"
activated in File -> Preferences.

bill.yu
Junior-7
Junior-7
Posts: 732
Joined: Mon Apr 02, 2018 11:05 am

Re: help

Post by bill.yu » Wed Aug 28, 2019 4:03 pm

Hi there~

Please double press the reset button on the board and see if the issue is solved. thanks.

ousmanedeme7313
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Sun Jan 13, 2019 11:12 pm

Re: help

Post by ousmanedeme7313 » Mon Sep 30, 2019 8:37 pm

Hello, I always have the same problem. can not the computer also cause worries? I have a dual core hp with windows 10.

Post Reply