Raspberry Pi And Rephone

Moderators: lily.li, violet, jessie, chao.zhang

Post Reply
contact8
Pre-kindergarten
Pre-kindergarten
Posts: 8
Joined: Sun Feb 14, 2016 4:32 am
Location: La Réunion

Raspberry Pi And Rephone

Post by contact8 » Sat Feb 27, 2016 9:28 pm

Hi,

I can't remember where in a video but I do remember of a picture of Raspberry Pi and a Rephone core module connected. UART, I2C ? May the dev team could give us a clue?

My point is to know if any one else is think about making these two new world opener talking together, even building together.

Let me explain my taught. I'm really looking for a light mobile dev environment since I met the Raspberry Pi.
My last working stuff is a Pi B with a PiTFT from Lady Ada and it's all battery powered in a cigar box. Completed with a wireless keyboard.
I'm looking to add a Rephone next to it to get a full next gen open stuff to work on.
Being on Reunion Island let me hope soon coding on the beach. ;-)

I started look at the LinkItAssist2502 makefile from Mandl but I can't figure out how to modify it to compile directly on the Pi which is already an Arm platform.

May someone like, want to work with me on that?

Have a love day.
Tropical Developer from Reunion Island

Re-Phone Create Kit + Expansion Pack
Raspberry Pi 2 (Raspbian)
Raspberry Pi B + Adafruit PiTFT

cord42
Pre-kindergarten
Pre-kindergarten
Posts: 4
Joined: Mon Jan 25, 2016 9:54 am

Re: Raspberry Pi And Rephone

Post by cord42 » Tue May 10, 2016 11:38 am

I also would like to know if anyone has had success with rephone and raspberry pi.

dbelam
Elementary-1
Elementary-1
Posts: 157
Joined: Wed Feb 03, 2016 2:59 am

Re: Raspberry Pi And Rephone

Post by dbelam » Wed May 11, 2016 3:00 am

You probably can't build on raspberry, sorry.
And to connect the 2? Probably uart, because the rephone only works As i2c master.

alexei.pavlov.goy
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sun Feb 14, 2016 3:12 am

Re: Raspberry Pi And Rephone

Post by alexei.pavlov.goy » Sat May 28, 2016 10:58 pm

Short question, did anyone connect raspberry pi with rephone? I don't mean the possiblity to build aplications from raspberry (raspbian). I mean the option to "capture" dates from rephone sending them to raspberry. Something like use the rephone as a "modem", for example to receive SMS...
Thank you

alexei.pavlov.goy
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Sun Feb 14, 2016 3:12 am

Re: Raspberry Pi And Rephone

Post by alexei.pavlov.goy » Sun Jun 05, 2016 5:59 am

Hi, guys,

Finally I could connect rephone to raspberry via modem. So now my raspberry receives SMS from rephone connected to raspberry and send them from raspberry. Using node.js framework, I even could send SMS with the shell command to raspberry, for example, send emails, create directories... Anything! Even something like "sudo reboot"...
So I confirm the rephone is a really very good device that works properly for raspberry (PI 3)
Now I would like to investigate a bit to know how to pair rephone to raspberry via bluethoot.

I anyone is interested how did I do it, please let me know, I would be happy to share it.

Best regards

Post Reply