(TECH) Incoming Ring Tone?

Moderators: lily.li, violet, jessie, chao.zhang

aea2
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Feb 25, 2016 12:05 pm

(TECH) Incoming Ring Tone?

Post by aea2 » Thu Feb 25, 2016 12:34 pm

Is there supposed to be a audible ring tone when there is an incoming call or sms? When I have an incoming call all I get is a screen that reads "incoming" with buttons to "reject" or "accept." When an sms comes in the screen turns on, but no sound.

seeed86
Pre-kindergarten
Pre-kindergarten
Posts: 37
Joined: Thu Feb 18, 2016 6:49 pm

Re: (TECH) Incoming Ring Tone?

Post by seeed86 » Thu Feb 25, 2016 4:15 pm

Actually, RePhone is a (kinda) opensource platform and you're free to edit CreateKit's source code as you wish.

Here is code, which is used to work with SMS.
Here is for playing audio.
And here is for voice calls.


And, as far as I see in the code, you're able to hook that events (incoming SMS and call) and play sound with ifttt thingie (green "If" icon in GUI interface on the LCD).

dbelam
Elementary-1
Elementary-1
Posts: 157
Joined: Wed Feb 03, 2016 2:59 am

Re: (TECH) Incoming Ring Tone?

Post by dbelam » Fri Feb 26, 2016 3:02 am

Or just copy your MP3 files in the root of the flash disk,
go to the "if" menu
and add 1-1 condition, that will play that MP3 when you get an SMS or get a call.

Consider: it won't stop playing, don't add a long MP3, or you will hear it all day! I'd recommend max 2-3 s length and strongly against cutting your favorite 40-50s from your dearest song.

aea2
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Thu Feb 25, 2016 12:05 pm

Re: (TECH) Incoming Ring Tone?

Post by aea2 » Fri Feb 26, 2016 3:25 am

Thanks for the notes. For now, I got it working by adding an mp3 and IFTTT.

sean7
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Tue Mar 01, 2016 10:36 pm

Re: (TECH) Incoming Ring Tone?

Post by sean7 » Tue Mar 01, 2016 10:38 pm

Hi- I too had this problem, so uploaded an MP3 file to the root of the flash memory, and used the IFTIST function but I still do not get a ring tone when calling.........any ideas?

dbelam
Elementary-1
Elementary-1
Posts: 157
Joined: Wed Feb 03, 2016 2:59 am

Re: (TECH) Incoming Ring Tone?

Post by dbelam » Wed Mar 02, 2016 3:12 am

If you go in the ifttt menu, does it appear in the list? I also messed up on first try, so maybe just did it wrong.

sean7
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Tue Mar 01, 2016 10:36 pm

Re: (TECH) Incoming Ring Tone?

Post by sean7 » Fri Mar 04, 2016 7:32 am

hi- yes it shows in the ifttt menu and the MP3 I downloaded to it shows in the memory, but it just wont play it manually or when there is an incoming call. ................help!

davidnoesunperro
Pre-kindergarten
Pre-kindergarten
Posts: 14
Joined: Mon Feb 22, 2016 4:32 pm

Re: (TECH) Incoming Ring Tone?

Post by davidnoesunperro » Fri Mar 04, 2016 9:17 pm

Hi there:
Just a lucky guess but...maybe the mp3's bitrate or frequency is too high to be played?
Try with a 128 Kpbs, maybe it'll work.
Keep us posted.

Best regards,
David.

dbelam
Elementary-1
Elementary-1
Posts: 157
Joined: Wed Feb 03, 2016 2:59 am

Re: (TECH) Incoming Ring Tone?

Post by dbelam » Sat Mar 05, 2016 1:30 am

My guess would be the file is too big - how many k-s it is in size?

sean7
Pre-kindergarten
Pre-kindergarten
Posts: 3
Joined: Tue Mar 01, 2016 10:36 pm

Re: (TECH) Incoming Ring Tone?

Post by sean7 » Sun Mar 06, 2016 6:36 pm

Hi all, its all working now, I think I made the mistake of unplugging the rephone from the computer without ejecting it as a drive. I erased my origin sound file, which was a complete tune, which although installed in the file system on the rephone board, would not play, even manually. I installed two different MP3 files and have one for text and one for ring tone notifications, and this all works fine now. I can only think unplugging the rephone without ejecting it on the computer caused corruption as sometimes happens on USB flash drives, fortunately its ok now.

Post Reply