thanks for your answer
so i make a lot of tests
but every times the same - the audio stops
it is the original audio example without a change
i changed one time the music.mp3, but the same happends
with and also without usb connect
my mp3 length is 6 sec
if i start the serial monitor
i see that the audio stops - no new messages
and i can start it again with key 1
Hi,
Audio paly can be interrupted by other task, for example a voice call.
Maybe you need check the audio status, and add the condition to resume play or restart.
There is the description about audio status in file “vmaudio.h”, from line 107 to 117.
Ths!