(TECH) Touchscreen Xadow connection clarifications

Moderators: lily.li, violet, jessie, chao.zhang

Post Reply
adam+seeed
Pre-kindergarten
Pre-kindergarten
Posts: 23
Joined: Sat Dec 05, 2015 8:43 am

(TECH) Touchscreen Xadow connection clarifications

Post by adam+seeed » Fri Jan 15, 2016 3:03 am

Hey all, I'm just wondering about a clarification.

On the Wiki page for the touchscreen ( http://www.seeedstudio.com/wiki/Xadow_1 ... ouchscreen ) the connectors are described as:
Connector:
2 × 35 PIN Xadow Connectors for Xadow GSM+BLE & Xadow Audio
So, is the "audio" side of the screen really just for audio only? And must the other side be connected only directly to the cellphone module? Are there pins that aren't passed-through the LCD, or is that merely talking specifically about and labeled for the "RePhone"-specific use of that screen?

Thanks!
Adam
[Edited to fix subject]
Last edited by adam+seeed on Mon Jan 18, 2016 1:46 am, edited 1 time in total.
----------
Keyboard for RePhone SMS messages:
Forum Thread: http://www.seeedstudio.com/forum/viewto ... 18&p=24134
GitHub Code: https://github.com/scriven42/RePhone_Cr ... ource_Code

kaktus.martin
Pre-kindergarten
Pre-kindergarten
Posts: 13
Joined: Tue Dec 29, 2015 9:33 pm

Re: Touchscreen Xadow connection clarifications

Post by kaktus.martin » Fri Jan 15, 2016 4:52 am

#A look at the datasheet would give you clarity... why people can't do that on your own?

Look at the attachment and post the answer at your own question...

adam+seeed
Pre-kindergarten
Pre-kindergarten
Posts: 23
Joined: Sat Dec 05, 2015 8:43 am

Re: Touchscreen Xadow connection clarifications

Post by adam+seeed » Fri Jan 15, 2016 10:42 am

I'm no expert, but to me the included attachment appears to show that it's a simple pass-through, and thus the labels were designed for RePhone Kit clarity and not as a limitation.

Maybe I was asking for _clarification_ because I wasn't an expert, and I thought these are meant to be helpful forums...RTFM isn't a smart or helpful answer, it's just a demonstration of an attitude.

Have a nice day.
----------
Keyboard for RePhone SMS messages:
Forum Thread: http://www.seeedstudio.com/forum/viewto ... 18&p=24134
GitHub Code: https://github.com/scriven42/RePhone_Cr ... ource_Code

User avatar
chao.zhang
Kindergarten
Kindergarten
Posts: 81
Joined: Thu Jan 22, 2015 9:55 am

Re: Touchscreen Xadow connection clarifications

Post by chao.zhang » Sun Jan 17, 2016 12:03 pm

adam+seeed wrote:Hey all, I'm just wondering about a clarification.

On the Wiki page for the touchscreen ( http://www.seeedstudio.com/wiki/Xadow_1 ... ouchscreen ) the connectors are described as:
Connector:
2 × 35 PIN Xadow Connectors for Xadow GSM+BLE & Xadow Audio
So, is the "audio" side of the screen really just for audio only? And must the other side be connected only directly to the cellphone module? Are there pins that aren't passed-through the LCD, or is that merely talking specifically about and labeled for the "RePhone"-specific use of that screen?

Thanks!
Adam
Hi Adam,

For clarification, all the modules with dual 35Pin connectors, such as Xadow 1.54'' touchscreen, Xadow Audio and Xadow GSM Breakout, they all have to be connected in the right orientation, check the following image:
Image

The Xadow 1.54'' touchscreen does not have unfilled corner, so instead you can regard the "phone" side as the starting end.

So the Xadow GSM+BLE has to be connected on the "phone" side, while the Xadow Audio and Xadow GSM Breakout are more flexible, and does not have to be on the "audio" side.

Post Reply