XADOW GPSv2

Moderators: lily.li, violet, jessie, chao.zhang

haugen.steinar
Pre-kindergarten
Pre-kindergarten
Posts: 7
Joined: Sun Jan 17, 2016 10:10 am

Re: XADOW GPSv2

Post by haugen.steinar » Sun Jan 17, 2016 12:11 pm

bakhdaulet wrote:I install Kinetis Design Studio 3.0.0 and KSDK_1.2.0 but Xadow source can't build & compile.
Can you write instruction like Arduino or Eclipse IDEs step by step how to use xadow source code on Kinetis Design Studio, may be need install drivers????????????
I opened all the files in the root of "..\xadow_phone_gps_v2" into an text-editor.
Find and Replace all D:\Freescale\KSDK_1.2.0 to your PATH
Find and Replace all D:\Freescale\WorkSpace\xadow_phone_gps_v2 to your PATH

Then:
05:10:01 **** Incremental Build of configuration Debug for project xadow_phone_gps_v2 ****
make all
'Invoking: Cross ARM GNU Print Size'
arm-none-eabi-size --format=berkeley "xadow_phone_gps_v2.elf"
text data bss dec hex filename
21724 132 1188 23044 5a04 xadow_phone_gps_v2.elf
'Finished building: xadow_phone_gps_v2.siz'
' '

05:10:02 Build Finished (took 1s.393ms)

bakhdaulet
Pre-kindergarten
Pre-kindergarten
Posts: 13
Joined: Tue Dec 29, 2015 11:58 am

Re: XADOW GPSv2

Post by bakhdaulet » Mon Jan 18, 2016 2:39 am

How to upload built source files to "Xadow GPSv2"?

bakhdaulet
Pre-kindergarten
Pre-kindergarten
Posts: 13
Joined: Tue Dec 29, 2015 11:58 am

Re: XADOW GPSv2

Post by bakhdaulet » Thu Jan 21, 2016 11:28 pm

Hi,
In XAdow GPSv2 Specification wrote about Power Saving
How to use 7uA@Backup Mode?????????????

bakhdaulet
Pre-kindergarten
Pre-kindergarten
Posts: 13
Joined: Tue Dec 29, 2015 11:58 am

Re: XADOW GPSv2

Post by bakhdaulet » Fri Jan 22, 2016 12:17 am

Could not connect to J-Link.
Please check power, connection and settings.SEGGER J-Link GDB Server V4.98b Command Line Version

JLinkARM.dll V4.98b (DLL compiled Apr 10 2015 20:15:52)

-----GDB Server start settings-----
GDBInit file: none
GDB Server Listening port: 2331
SWO raw output listening port: 2332
Terminal I/O port: 2333
Accept remote connection: localhost only
Generate logfile: off
Verify download: on
Init regs on start: on
Silent mode: off
Single run mode: on
Target connection timeout: 0 ms
------J-Link related settings------
J-Link Host interface: USB
J-Link script: none
J-Link settings file: none
------Target related settings------
Target device: MKL02Z32xxx4
Target interface: SWD
Target interface speed: 1000kHz
Target endian: little

Connecting to J-Link...
Connecting to J-Link failed. Connected correctly?
GDBServer will be closed...
Shutting down...




----------------------------------------------------------------------------------
Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect 'cmsis-dap'
Error: unable to open CMSIS-DAP device
Error: unable to init CMSIS-DAP driver
Error: Error selecting 'cmsis-dap' as transport
Runtime Error: C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg:3:
in procedure 'script'
at file "embedded:startup.tcl", line 58
in procedure 'interface' called at file "C:/Freescale/KDS_3.0.0/openocd/bin/..//scripts/kinetis.cfg", line 3

Post Reply