Page 1 of 1

Using 10.1" IPS LCD display

Posted: Mon Jun 03, 2019 5:42 am
by rogferd50
I recently purchased one of the non-touch 10.1" displays (https://www.seeedstudio.com/10-1-inch-1 ... -2863.html), and the control buttons do nothing. When power is applied, it comes on a full brightness, and that's it. The power button doesn't turn it on or off, and the increase/decrease brightness buttons also do nothing. I've driving it with a Raspberry Pi 3 A+.

Is there some configuration I need to do on the display itself in order to enable the buttons? Any advice would be greatly appreciated.

Lot of beautiful faces

Posted: Wed Jun 12, 2019 12:04 am
by trippwainwright
What as up, just wanted to say, I loved this article. It was funny. Keep on posting free bigtits hardcore!