Longan Nano

General information

Moderators: lily.li, violet

Post Reply
william.quartz
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Wed Apr 24, 2019 8:12 pm

Longan Nano

Post by william.quartz » Wed Oct 09, 2019 2:55 am

Hi,

Is there anyone that can help me setup my Longan Nano under PlatformIO? I can build the blink example but I can't upload.
I have the sipeed-rv-debugger connected but maybe I don't have it wired correctly.
Each time I try to "upload" I get a strange error:

Code: Select all

Processing sipeed-longan-nano (platform: gd32v; board: sipeed-longan-nano; framework: gd32vf103-sdk; board_build.mcu: GD32VF103CBT6; board_build.f_cpu: 108000000L)
----------------------------------------------------------------------------------------------------------------------------------------
CONFIGURATION: https://docs.platformio.org/page/boards/gd32v/sipeed-longan-nano.html
PLATFORM: GigaDevice GD32V 1.0.0 > Sipeed Longan Nano
HARDWARE: GD32VF103CBT6 108MHz, 32KB RAM, 128KB Flash
DEBUG: Current (altera-usb-blaster) External (altera-usb-blaster, gd-link, jlink, sipeed-rv-debugger, um232h)
PACKAGES: toolchain-gd32v 9.2.0, tool-openocd-gd32v 0.1.1, framework-gd32vf103-sdk 1.0.0, tool-gd32vflash 0.1.0
LDF: Library Dependency Finder -> http://bit.ly/configure-pio-ldf
LDF Modes: Finder ~ chain, Compatibility ~ soft
Found 0 compatible libraries
Scanning dependencies...
No dependencies
MethodWrapper(["checkprogsize"], [".pio/build/sipeed-longan-nano/firmware.elf"])
Memory Usage -> http://bit.ly/pio-memory-usage
DATA:    [=         ]   7.0% (used 2310 bytes from 32768 bytes)
PROGRAM: [=         ]   5.0% (used 6572 bytes from 131072 bytes)
text       data     bss     dec     hex filename
   6460     112    2198    8770    2242 .pio/build/sipeed-longan-nano/firmware.elf
<lambda>(["upload"], [".pio/build/sipeed-longan-nano/firmware.bin"])
AVAILABLE: altera-usb-blaster, gd-link, jlink, serial, sipeed-rv-debugger, um232h
CURRENT: upload_protocol = serial
MethodWrapper(["upload"], [".pio/build/sipeed-longan-nano/firmware.bin"])
Auto-detected: /dev/ttyUSB0
stm32flash -g 0x08000000 -b 115200 -w ".pio/build/sipeed-longan-nano/firmware.bin" "/dev/ttyUSB0"
Failed to init device.
stm32flash Arduino_STM32_0.9

http://github.com/rogerclarkmelbourne/arduino_stm32

Using Parser : Raw BINARY
Interface serial_posix: 115200 8E1

*** [upload] Error 1
My .ini file is:

Code: Select all

[env:sipeed-longan-nano]
platform = gd32v
board = sipeed-longan-nano
framework = gd32vf103-sdk
; change microcontroller
board_build.mcu = GD32VF103CBT6

; change MCU frequency
board_build.f_cpu = 108000000L
Any ideas? Thanks.

FYI, my lcd display only display a white background on the device, not sure if that is normal.

bigbits
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Sep 24, 2019 10:42 am

Re: Longan Nano

Post by bigbits » Sat Oct 12, 2019 11:23 am

Hi,

It seems that you did not choose the correct upload_protocol.

If you use a serial port to connect to a longan board, you need to specify

Code: Select all

upload_protocol = serial
upload_port = /dev/ttyUSB1 ; If you have both /dev/ttyUSB0 and /dev/ttyUSB1, select /dev/ttyUSB1
If you use jtag to connect, need to specify

Code: Select all

upload_protocol = sipeed-rv-debugger

The complete configuration file looks like this:

Code: Select all

[env:sipeed-longan-nano]
platform = gd32v          ; Platform, choose gd32v
framework = arduino       ; Optional gd32vf103-sdk or arduino
board = sipeed-longan-nano ; Development board
monitor_speed = 115200     ; Serial monitor baudrate
upload_protocol= serial       ; Download tool Default serial port, optional jlink, gd-link, dfu, sipeed-rv-debugger,etc.
upload_port = /dev/ttyUSB1 ; If you have both /dev/ttyUSB0 and /dev/ttyUSB1, select /dev/ttyUSB1
debug_tool = sipeed-rv-debugger         ; Debugging tool default jlink, optional sipeed-rv-debugger, etc.
You can find more information at our WIKI.https://longan.sipeed.com/en/get_started/blink.html

Post Reply