Using 10.1" IPS LCD display

General information

Moderators: lily.li, violet

Post Reply
rogferd50
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Sat May 18, 2019 12:17 am

Using 10.1" IPS LCD display

Post by rogferd50 » Mon Jun 03, 2019 5:42 am

I recently purchased one of the non-touch 10.1" displays (https://www.seeedstudio.com/10-1-inch-1 ... -2863.html), and the control buttons do nothing. When power is applied, it comes on a full brightness, and that's it. The power button doesn't turn it on or off, and the increase/decrease brightness buttons also do nothing. I've driving it with a Raspberry Pi 3 A+.

Is there some configuration I need to do on the display itself in order to enable the buttons? Any advice would be greatly appreciated.

trippwainwright
Pre-kindergarten
Pre-kindergarten
Posts: 2
Joined: Tue Jun 11, 2019 11:58 pm

Lot of beautiful faces

Post by trippwainwright » Wed Jun 12, 2019 12:04 am

What as up, just wanted to say, I loved this article. It was funny. Keep on posting free bigtits hardcore!

Post Reply