Store settings without the battery.

Moderators: lily.li, violet, jeremy882, crail.lyu969

Post Reply
Smoking
Pre-kindergarten
Pre-kindergarten
Posts: 1
Joined: Wed Apr 07, 2010 4:11 pm

Store settings without the battery.

Post by Smoking » Wed Apr 07, 2010 4:15 pm

Hi all,
is it possible to store the settings without a battery.
I don't want to use the battery only an external power but when the power goes off the settings are gone.
Is there a way to over come this?

Thankx

FreeZinG

Re: Store settings without the battery.

Post by FreeZinG » Sat Apr 10, 2010 9:55 am

The setting is saved of the SD card (old version firmware) or the Flash (new version) , so even you use the USB power , when power off , the setting will still store in the DSO .

We will add a selection to choose save the setting on sd card or flash next version firmware.

Post Reply