What can i do with the "config.dat"

Moderators: lily.li, salmanfarisvp, violet, jeremy882, crail.lyu969

Post Reply
ms-test-9999
Pre-kindergarten
Pre-kindergarten
Posts: 9
Joined: Sat Jan 09, 2010 10:51 am

What can i do with the "config.dat"

Post by ms-test-9999 » Mon Jan 25, 2010 5:36 am

What are the information that are stored in this "config.dat" on the SD-card ?

It is not readable with an texteditor, so how can i edit it, what are the structure of it ?

Has anybody got more information about this topic ?

Thanks in advance ...

FreeZinG

Re: What can i do with the "config.dat"

Post by FreeZinG » Mon Jan 25, 2010 9:39 am

The new F/W save the config.dat in the FLASH in the STM32 instead of the card .

ms-test-9999
Pre-kindergarten
Pre-kindergarten
Posts: 9
Joined: Sat Jan 09, 2010 10:51 am

Re: What can i do with the "config.dat"

Post by ms-test-9999 » Sat Jan 30, 2010 10:03 am

The new F/W has a config screen and an option like:

"Save settings at power-down" ON oder OFF.

I like ON.

Post Reply